Skip to main content
Renesas Electronics Corporation

Description

This board extends the function of R-Car Starter Kit Premier/Pro, equipped with up to 8 cameras, Wi-Fi/BT, CAN, Multi Audio and various other functions. This enables richer in-vehicle application development such as integrated cockpit domain controllers, in-vehicle infotainment, digital instrument clusters and driver-monitoring systems.

Applications

Support Communities

  1. NVMe drive not detected on ( R-Car H3e-2G Starter Kit + SBEV-RCAR-KF-M06 )

    Hi All,   We are currently trying to use AGL OS on the board “R-Car H3e-2G Starter Kit + Kingfisher Infotainment Board”. Successfully booted up using the prebuilt image with SD card.   But when connected an SSD drive to the M.2 slot on Kingfisher board, it  does not detect ...

    Oct 26, 2022
  2. NVMe drive not detected on ( R-Car H3e-2G Starter Kit + SBEV-RCAR-KF-M06 )

    Hi All,   We are currently trying to use AGL OS on the board “R-Car H3e-2G Starter Kit + Kingfisher Infotainment Board”. Successfully booted up using the prebuilt image with SD card.   But when connected an SSD drive to the M.2 slot on Kingfisher board, it  does not detect ...

    Oct 26, 2022
  3. R-Car H3 SK + KF Camera interface

    Hi,     We have H3 SK (RTP0RC77951SKBX010SA03, 8GiB(Samsung 2GB x4), Single Rank) and KF (SBEV-RCAR-KF-M06Board).     And we have LI-IMX219-MIPI-FF-NANO-H136 camera sensor module and trying to interface with RCar -H3 SK + KF platform.    We followed R-Car/Boards/Yocto-Gen3/ ...

    Jun 18, 2021
View All Results from Support Communities (6)