Skip to main content
Renesas Electronics Corporation

Overview

Description

The Renesas Starter Kit for RX63T (64-pin) is intended as a user-friendly introductory and evaluation tool for the RX63T microcontroller. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop.

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Applications

Documentation

Design & Development

Software & Tools

Software Downloads

Sample Code