Skip to main content
Renesas Electronics Corporation

Description

The Renesas Starter Kit for RX610 is intended as a user-friendly introductory and evaluation tool for the RX610 microcontroller. The board also provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop as well as programming the device using E1 emulator and/or Flash Development Toolkit.

The Renesas Starter Kit for RX610 may be connected to the host PC using a simple RS232 serial connection or via the included USB E1 on chip debugging interface.

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Applications

Type Title Date
Application Note PDF 358 KB 日本語
AI-generated Summary: The document explains how to manage sub-projects in CubeSuite+ by deleting unused ones to optimize the build process. It details changing and setting properties of the RX E1(JTAG) debug tool, including clock frequency and power supply settings. Instructions cover building the project, starting the E1 emulator, handling warning messages related to operating frequency, and executing the program after download.
Application Note PDF 354 KB 日本語
AI-generated Summary: The RX610 Renesas Starter Kit sample code includes source files such as main.c, which contains the main() function displaying the Renesas splash screen and running LED and timer functions. The code is designed for the RSK but serves as a useful example even without it. General precautions for handling Renesas MPU/MCU products emphasize proper handling of unused pins, stable clock signals before releasing reset, prohibition of accessing reserved addresses, and verifying differences when switching products. The document also provides Renesas website and inquiry links for support.
PCB Design Files
Log in to Download ZIP 902 KB 日本語
Manual - Development Tools PDF 89 KB
Manual - Development Tools PDF 372 KB 日本語
Manual - Development Tools PDF 517 KB 日本語
Manual - Development Tools PDF 365 KB 日本語
Manual - Development Tools PDF 293 KB 日本語
8 items

Software & Tools

Software Downloads

Type Title Date
Software & Tools - Evaluation Software
Log in to Download ZIP 37.73 MB 日本語
Software & Tools - Evaluation Software
Log in to Download ZIP 38.46 MB 日本語
Upgrade - Debugger
Log in to Download ZIP 110.84 MB 日本語
Software & Tools - Evaluation Software
Log in to Download ZIP 122.90 MB 日本語
Software & Tools - Other
Log in to Download ZIP 230.12 MB
5 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 5.98 MB 日本語 IDE: CS+
Sample Code
Log in to Download ZIP 36.99 MB 日本語 IDE: HEW
2 items
Part NumberStatusStockSampleable
R0K556100S000BEObsoleteOut of StockN/A

Support Communities

  1. about simple code in c for microcontroller

    can anybody help me??I want simple code using c to help me for understanding how i can use  registers to transfer data on specific portthe example about anything likepush button when I pressed on it the led flashed

    Dec 31, 2010