Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

LTE IoT includes the very latest cellular technologies, Cat-M1 and Cat-NB1 (NB-IoT), both are ideal for connecting IoT devices and sensors to 4G LTE cellular networks globally. AE-CLOUD2 enables the connection of those IoT devices to cloud service providers with minimal effort.

AE-CLOUD2 can be used anywhere in the world, as it has support for Cat-M1, Cat-NB1, 2G/EGPRS, as well as GPS. The kit complies with global regulatory certifications for FCC, CE, RoHS, WEEE, and Japan MIC. The AE-CLOUD2 kit has been designed to work with CAT-M and NB-IoT networks. Users should check that these networks are supported by cellular providers in their region and have the ability to configure the modem to establish a connection to an available regional network through a local cellular provider.

System Requirements

The Synergy™ Enterprise Cloud Toolbox is no longer available. Please see the cloud-specific Cloud Connectivity Application Projects to connect to specific cloud service providers.

Features

  • Enables rapid evaluation, prototyping, and development of global LTE IoT cloud-connected applications using the Synergy Platform
  • Supports cellular IoT protocols:
    • Cat-M1
    • Cat-NB1
  • Easily connects IoT sensor devices to major cloud services worldwide
  • Powered by the S5D9 MCU Group, the superset of the S5 MCU series
  • Includes a wide variety of onboard sensors:
    • Lighting sensor
    • Microphone
    • Temperature sensor
    • Humidity sensor
    • Pressure sensor
    • Air quality sensor
    • Geomagnetic sensor
    • Accelerometer
    • Gyroscope

Applications

Documentation

Design & Development

Sample Code

Product Options

Part NumberStatusStockSampleablePb (Lead) FreeECCN (US)HTS (US)RoHS CompliantChina RoHS Compliant
RTK7AECLD2S00001BUObsoleteIn StockN/ANo3A991.a.28471.50.0150NoNo
YSAECLOUD2NRNDIn StockN/ANo3A991.a.28471.50.0150NoNo

Support

Support Communities

  1. Synergy MQTT/TLS AWS Cloud Connectivity Sample Code Fails to Build

    ... unsupported SSP version. Use e² studio 2022-07 or earlier to either continue using this project or to upgrade it to SSP 2.0.0 or later ". Please let me know how to proceed at the earliest. www.renesas.com/.../rtk7aecld2s00001bu-ae-cloud2-global-lte-iot-connectivity-example

    Dec 18, 2024