Skip to main content
Renesas Electronics Corporation

Description

This kit has been discontinued. The successor to this kit is M16C/6S1 Group Evaluation Kit : EV10.

Features

  • Includes 1 complete PLC nodes with FCC band
  • Includes an AC/DC Adapter
  • Includes the example simple communication test program
  • Includes a serial cross over cable
  • The Differences between EV5 FCC and EV5 ASIA are AC/DC Adapter and AC cables

Applications

Type Title Date
Manual - Development Tools PDF 543 KB
1 item
Part NumberStatusStockSampleable
R0K3306S0D010BRObsoleteOut of StockN/A

Resources

Knowledge Base

  1. What to do when I get an error on ID code and can't continue programming?

    The M16C Flash Starter always requires an ID code. You always need to enter an ID code to be able to program a blank Flash memory. The ID code can be any value for a blank Flash memory but you cannot leave it blank.

    Feb 14, 2006
  2. What will be written in the ID code area without setting the value?

    When programming the on-chip Flash memory without setting a value in the ID code area, the M16C Flash Starter will set "FF FF FF FF FF FF FF" in the ID code area. Therefore, the next time you reprogram the Flash memory, input [all "FFh"] to verify the ID ...

    Feb 14, 2008
  3. What is the matter why can't I program the memory using "00h" as ID code?

    The ID you enter is used to 'unlock' the device so you can program it. It is NOT the ID that will be programmed on the device. The ID code changes according to the contents written to the on-chip Flash memory during the previous programming session. You should know ...

    Feb 14, 2008
View All Results from Knowledge Base (5)