Skip to main content

Overview

Description

The I/O DLL kit provides a means for extending the functions of the simulator debugger in the High-performance Embedded Workshop integrated development environment (IDE). This kit supports the creation of I/O DLLs. The I/O DLL refers to a DLL (Note1) that operates in cooperation with the simulator engine of the simulator debugger.

Once the necessary settings are made, the simulator debugger allows you to load an I/O DLL and operate it synchronously with the timing at which instructions are single-stepped, memory is read or written or an interrupt occurs. That way, the operation of the input/output ports or the internal peripheral functions of the microcomputer can be simulated as a means of debugging the target program. Furthermore, linked operation with an external tool can be realized by, for example, sending and receiving data to and from that tool.

Any desired I/O DLL can be created by using C/C++ language. To create an I/O DLL, you need to have Microsoft Visual C++, a Windows application development environment available on the market.

Note

  1. DLL is the acronym of Dynamic Link Library. This is a function of the operating system that allows you to save executable routines (routines that supply a specific function or a set of functions) to be saved separately as a file with the extension ".dll". These routines are loaded only when they are needed by the calling program.

Learn More

Target Devices

Downloads

Documentation

Support

Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?

Additional Details

Linkage Between the Simulator Engine and I/O DLL

The simulator engine calls the functions that have been predefined on the I/O DLL side synchronously with the timing shown below:

  • After executing one instruction (number of execution cycles)
  • Before execution (PC value)
  • When the target is reset
  • When an interrupt occurs
  • Immediately before memory read (address information)
  • Immediately after memory write (address information)

Conversely, the following functions that have been made public for the simulator engine can be called from the I/O DLL side:

  • Get memory contents
  • Set a memory value
  • Get a register value
  • Set a register value
  • Interrupt occurrence
  • Confirm interrupt occurrence condition
  • Inspect the total number of cycles executed
Image
Processing flow

Processing flow

Supported Simulator Debuggers

This I/O DLL kit is available for the following simulator debuggers in the compiler packages :

Note: This I/O DLL kit is NOT supported by the M3T-PDxxSIM simulator debuggers. For M3T-PDxxSIM, use the PDxxSIM I/O DLL Kit.

Development Tools Used

To create an I/O DLL, you need to have Microsoft Visual C++, a Windows application development environment available on the market.

Sample Programs

The following sample programs are stored in a location at the hierarchical level below the directory in which this I/O DLL kit is installed. Refer to the release note for details on how to install the I/O DLL kit.

  • I/O DLL to link with Excel from Microsoft Corporation
  • I/O DLL to read/write data from a file
  • I/O DLL to simulate the operation of a microcomputer's internal peripheral functions