Skip to main content
Renesas Electronics Corporation

SMART Modular Selects IDT as a Preferred Partner for DDR4 NVDIMM Technology

IDT’s DDR4 NVDIMM Chipset—Featuring Registered Clock Driver, Thermal Sensor and Multiplexers—Is the Only Complete NVDIMM Solution on the Market

October 23, 2015

 SAN JOSE, Calif., Oct. 23, 2015— Integrated Device Technology, Inc.® (IDT®)  (NASDAQ: IDTI) today announced that SMART Modular Technologies®, a global leader in specialty memory solutions, has chosen IDT as a preferred partner for its DDR4 NVDIMM (non-volatile dual in-line memory module) product. The new offering includes the 4RCD0124K registered clock driver (RCD) and TSE2004GB2 thermal sensor with SPD, which are part of IDT’s NVDIMM chipset. The chipset is the only complete DDR4 NVDIMM solution available on the market and has been customer qualified and OEM validated.

NVDIMM technology delivers DRAM performance along with data persistence in the event of power loss by providing a mechanism to back up data from DRAM to non-volatile memory. NVDIMMs are installed into existing DIMM sockets in a system and are often heterogeneously populated alongside standard DIMMs.  Without compromising the signal integrity of the motherboard channel, IDT’s high-performance multiplexer technology delivers fast, glitch-free bus-switching capabilities between system and local controllers on an NVDIMM.  NVDIMMs utilizing the IDT chipset can deliver maximum performance and extreme reliability in multi-slot server systems.

“The NVDIMM market is poised for strong growth as new applications and usage models emerge in the datacenter, enterprise and storage markets,” said Srida Joisa, senior director of SMART’s DRAM Product Line. “SMART is fully invested in the NVDIMM market and is excited to have IDT on as a preferred memory interface supplier for DDR4 NVDIMMs.”

“SMART Modular is a valued IDT customer, and we are pleased to be a preferred partner to enable their NVDIMMs with our industry-proven chipset,” said Rami Sethi, vice president and general manager of IDT’s Memory Interface Products. “NVDIMM is a fast-emerging technology for server and storage systems, and IDT has been at the forefront of it with our full suite of DDR4 product offerings.”

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc.  All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.