2017年11月10日
このビデオについて
Introducing the ISL78226, the industry's first 6-phase bidirectional PWM controller designed to perform buck and boost power conversions between 12V and 48V automotive buses. The ISL78226's high integration and innovative features simplify designing a robust 48V/12V power net solution for automakers. Designers don't have to be digital power experts or assemble multiple buck and boost controllers to create a 48V mild hybrid design.