概要
The SLG59M1457V evaluation board evaluates the SLG59M1457V GreenFET single N-channel load switch, enabling validation of its switching performance and power management functionality. Dedicated sense test points support precise RDS(on) characterization during device testing. These test points are intended for evaluation purposes only and are not designed to carry high currents.
For details on how to use the evaluation board, please refer to the evaluation board user manual included in the datasheet.
使用製品
サンプル&ご購入