メインコンテンツに移動

ブログ

Energy-Efficient Motor Control for Home Appliances Blog

Energy-Efficient Motor Control for Home Appliances

This blog presents a market overview of the motors used in consumer appliances, energy optimization challenges, and the Renesas MCU infrastructure supporting motor control applications in consumer appliances.

NFC Revolutionizing IoT Applications: A Seamless Future Blog

NFC Revolutionizing IoT Applications: A Seamless Future

Embrace the future of connectivity and enhance your application with Renesas' PTX105R NFC controller for Internet of Things applications, the most suitable NFC reader on the market.

Renesas QEMU Environment is a simulator for R-Car S4 that achieves high-speed simulation

高速なシミュレーションを実現するR-Car S4用シミュレータRenesas QEMU Environment

高速なシミュレーションを実現するR-Car S4用シミュレータRenesas QEMU Environmentをご紹介します。

AI Coding with ChatGPT for RL78 Microcontrollers (Arduino)

Chat-GPTを利用したRL78マイコンのAIコーディング (Arduino)

このブログでは、Chat-GPTとRL78 Arduino互換ボードを使用してAIコーディングを行う方法と、その実例を紹介します。

 The IoT Cloud Connection Decision: Wi-Fi or Cellular?

The IoT Cloud Connection Decision: Wi-Fi or Cellular?

With the ubiquity of wireless connectivity options on IoT devices, connection to the cloud has become more flexible than ever. Traditionally, Wi-Fi has been the most popular choice in the IoT world although this has changed in recent years with the huge strides made in cellular networks. However, there is no right answer for which option would be the best or the more efficient between the two.

The type of network connection to use depends on several factors that affect solution development.

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

The AIoT has been enabled by higher MCU compute capability and thin neural network models that are more suited for edge and end point devices than traditional CPUs and MPUs.

Renesas Initiatives in Smart Agriculture - Part 1

スマート農業におけるルネサスの取り組み~Part1

スマート農業を実現するためのルネサスソリューションの紹介

Closing the Performance Gap Between DRAM and AI Processors

AIプロセッサとDRAMの性能ギャップを埋める

ルネサスのメモリインタフェースが果たす役割をご紹介します。

Let's Create a Digital Angle Meter Using a Microcontroller

マイコンを使ってデジタル角度計を作ろう!

RL78/G15 Fast Prototyping Boardを使用して、デジタル角度計を作成します。ジャイロセンサから得られたデータを角度に変換し、LCDに表示します。ジャイロセンサからのデータ受信、LCDへのデータ送信は、I2C通信で行います。

Introducing An Easy Tool for Touch Development Even with Partner IDE Platforms

パートナー製の統合開発環境でも簡単にタッチ機能を開発できるツールのご紹介

スタンドアローン版QE for Capacitive Touchを使用することで、IAR社のEWRXでも静電容量式タッチセンサの開発が可能となります。