メインコンテンツに移動

ブログ

Improve UX/UI with RX140 MCU Equipped with A New Generation of Capacitive Touch Sensor

UX/UIを改善する新世代の静電容量式タッチセンサ搭載マイコン「RX140」

RX100シリーズの新製品RX140は機器の性能アップと低消費電力化の両立に加え、最新のタッチキーIPを搭載し、お客様製品のさらなるデザイン性やユーザビリティの向上に貢献します。

What is data acquisition (DAQ) and distributed processing/edge computing in the IoT era with RX23E-A?

RX23E-AによるIoT時代のデータアクイジション(DAQ)と分散処理/エッジコンピューティングとは?

高精度AFE内蔵マイコンRX23E-Aと産業ネットワーク機能を強化したマイコンRX72Mを組み合わせることで、IoT時代にマッチしたデータアクイジション(DAQ)を実現することが可能です。

Dataline performance of two new actors in the networking arena

The Art of Networking (Series 4): CAN XL and 10BASE-T1S – Dataline Performance of Two New Actors in the Networking Arena

This blog gives a brief overview of CAN XL and 10MBit/s Ethernet, and the differences between them.

Functional Safety over EtherCAT Blog

ルネサスによる、Functional Safety over EtherCATへの取り組み

ルネサスが2020年後半にFSoEソリューションを発売して以来、このソリューションは世界中から注目されています。このブログでは、ルネサスのFSoEソリューションがどのように開発を容易にし、且つ開発期間を短縮するのかをご紹介します。

Obtain the Latest Information at the “Virtual Renesas Automotive Days”!

「Renesas Automotive Days オンライン」で最新情報をご入手ください!

“ルネサスの戦略と幅広い車載ソリューションラインナップをアップデートさせていただく機会として「Renesas Automotive Daysオンライン」を開催します。

RX72M Single-Chip Motor Control via EtherCAT Communications

RX72M EtherCAT 通信を用いたシングルチップソリューション

ルネサスはアプリケーション処理と標準的なEtherCAT通信、モータ制御をワンチップで実現するRX72M モータ+EtherCAT シングルチップソリューションをご提案します。

The RX671 Microcontroller Meets the Ever-evolving Demands of IoT Devices Blog

進化し続けるIoT機器の要求にお応えする新製品RX671

家電や産業機器の進化・IoT化に貢献してきたRX600シリーズに新製品RX671が加わりました。演算能力・機能が強化されたRX671の追加で、より幅広いニーズへの対応が可能となりました。

Ka-band Rx Beamforming IC Blog

Successful Demonstration of Next-Gen Ka-band Rx Beamforming IC Portfolio with 1.5dB NF LNA

This blog provides an overview of the Ka Satcom band LNA lab demo that achieved a new performance benchmark for active beamforming ICs in electronically steered phased array antennas with two simultaneous beams.

The Art of Networking (Series 3): The Power of Virtualization Blog

ネットワーク技術(シリーズ3):仮想化の力

ソフトウェアによる仮想化はECU統合の用途において強力なツールの1つです。本稿では、2つの仮想マシン間でデータを共有するケースにおいて、①ソフトウェアのみで実現した場合と、②仮想化支援機能を持つ車載イーサネットスイッチを用いた場合について、その比較結果を示します。仮想化を支援する周辺機能(ハードウェア)は、仮想化に伴うオーバーヘッドの低減に貢献します。

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Renesas’ Lab on the Cloud bridges the gap between ordering evaluation boards and testing in the lab by providing access to live boards in a physical lab through an online interface.