Skip to main content

Renesas Blog

Quickly Programming RA MCU Innovation Kits for IoT

Quickly Programming RA MCU Innovation Kits for IoT

This blog provides useful information on programming a pre-built hex file onto an RA kit using Renesas Flash Programmer and Segger® J-Flash Lite without having to build the source code or use an IDE.

hybrid, power line communication plus sub-GHz RF reference platform (Y-G-HYBRID-PLC-RF)

Renesas Launches its First Hybrid Reference Platform Combining Power Line Communication and Sub-GHz Radio

Renesas’ first hybrid, power line plus sub-GHz RF reference platform is a reference board that supports all key communication protocols such as WiSUN, G3-PLC, G3-PLC Hybrid, PRIME 1.3.6 + 1.4, PRIME Hybrid and Meters and More.

What is Driving DDR5? Blog

What is Driving DDR5?

This blog goes over the need for faster and more memory and how DDR5 is addressing this need.

The RA MCU family is made to help solve your design challenges

The RA MCU Family is Made to Help Solve Your Design Challenges

The entry-level RA4E1 and RA6E1 MCUs address key design challenges including the optimal balance between performance and power consumption, as well as seamless migration options for future designs.

RA Book Features Blog

Get Where You’re Going with the Official Renesas RA Family Guide

This blog presents the RA Family Beginner’s Guide – A step-by-step guide that takes you from the basics of the FSP and RA toolchain to creating a project from scratch with the EK-RA6M4 evaluation kit.

Robotic Lawn Mower Blog

Lawn Maintenance Getting You Down? Robotic Mowers to the Rescue!

Compared to conventional lawn mowers, robotic lawn mowers offer many benefits including they are better for our environment and offer the convenience of remote programming, controlling and monitoring.

RapidCharge™ Controllers Prevent Fast Charger Hacking Blog

RapidCharge™ Controllers Prevent Fast Charger Hacking

Fast chargers and power supplies designed with Renesas' Rapid Charge™ controllers cannot be hacked, because they are hard-wired state machines that have no firmware that can be accessed and corrupted.

Ultimate optimization from custom ASICs

5 Things You May Not Know About an ASIC

There are many advantages to having an ASIC developed for your next product. Some of these advantages might be new to you. Here, we detail five of the lesser-known benefits.

ForgeFPGA

A New Era for Programmable Logic

There are many applications where a small amount of programmable logic can be useful, especially if the pricing is attractive. To address this gap, we have introduced a new line of low-density FPGAs.

Beacon blog

Beacon, Tag, or Both?

While the underlying technology is the same, the way beacons and tags are used is quite different, and understanding those differences leads to powerful new applications for consumers.