Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Advanced Lasting Data-Retention Endurance Without Battery Back-Up

Advanced Lasting Data-Retention Endurance Without Battery Back-Up
May 14, 2026

About This Video

Unlike conventional RAM technologies that store data as electrical charge or current, MRAM uses magnetic domains to retain data without power — and this webinar examines what that fundamental difference means for system designers. Covering how MRAM compares to other non-volatile memory technologies across the parameters that matter most — power consumption, access speed, endurance, and data retention — the session introduces the Renesas M1000/M3000 family as a next-generation solution offering more than 20 years of data retention alongside large memory density. A practical overview for designers evaluating non-volatile memory options where battery-backed solutions are undesirable or impractical.