Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

IAR Systems

IAR Embedded Workbench®, the world’s most widely used embedded development environment, is fully integrated with the Synergy™ Platform.

IAR Embedded Workbench for Renesas Synergy offers tools for efficient code development, including a highly optimizing C/C++ compiler and linker, and C-STAT® Static Analysis and C-RUN® Runtime Analysis tools that allow developers to find potential code issues early in the development process. The Power Debugging tool helps developers understand how code changes affect power consumption.

IAR Embedded Workbench for Renesas Synergy interfaces with the Synergy Standalone Configurator (SSC), a standalone tool created by Renesas. The SSC includes a project editor with configurators such as the Clock Configurator, Pin Configurator, RTOS Configurator, and Synergy Software Package (SSP) Module Configurator. IAR Embedded Workbench for Renesas Synergy also allows visibility into protected SSP code, helping developers understand the inner workings of the SSP while debugging.

Release Information

Download Information

IAR Embedded Workbench for Synergy (EWSYN) is no longer available for download from Renesas.com. Contact IAR for access to the Embedded Workbench for Synergy. Licenses for EWSYN are issued by IAR, users can find additional information on licensing Embedded Workbench for Synergy and request a new or updated license key from IAR from the IAR Embedded Workbench for Renesas Synergy webpage.

Installation Instructions

For detailed installation instructions on how to install IAR Embedded Workbench for Synergy, refer to the release note for IAR Embedded Workbench for Renesas Synergy v8.23.3, available for download from the Synergy Standalone Configurator (SSC) product page on Renesas.com.

Target Devices

Support Communities

  1. Introducing the IAR Embedded Workbench® for Renesas Synergy™

    ... when compared to a professional tool such as the IAR Embedded Workbench® for Renesas Synergy™ which is now included in the Renesas Synergy™ Platform.   Developers using the Synergy Platform now have the choice to use E2 studio, an Eclipse based Integrated Solution Development Environment using GCC for ...

    Aug 11, 2016
  2. Switching from e2 Studio to IAR Embedded Workbench® for Renesas Synergy™

    For some time now, the Synergy Platform has had the IAR Embedded Workbench® for Renesas Synergy ™ development environment and compiler available to developers. Engineers that have been using e2 Studio might be hesitant to convert their e2 projects into IAR Workbench projects. Doesn’t this seem like it ...

    Jan 26, 2017
  3. Lowering Barriers to Entry

    ... teams’ energy and creativity. My favorite example is how Synergy Platform users have access to high quality, commercial-grade tools and software such as the IAR Embedded Workbench® for Synergy and the Synergy Software Package (SSP). Using this commercial software allows a team to leverage existing and proven application ...

    Aug 10, 2016