Overview
Description
Flash memory reprogramming software for RL78/L23 has been released.
The data flash library is free-of-charge software that reprograms the contents of the data flash memory by user programs.
"Renesas Flash Driver for RL78" is free-of-charge software that reprograms the contents of code flash memory and data flash memory by user programs.
Features
- Data Flash Libraries provide the interface for operations on the areas of data flash memories that MCUs have. (Functions are supported varies with the MCU. Please check the available functions in the user's manual for the target flash reprogramming software.) :
- Erasing
- Programming
- Internal verification
- Blank checking, etc.
- An EEPROM emulation library for data flash memory is also included.
- Learn More
Release Information
Renesas Flash Driver RL78 Type 11 for RL78/L23 Group
- Latest Ver.: Ver.1.00
- Released: Sep 05, 2025
EEPROM Emulation Software RL78 Type 11 for RL78/L23 Group
- Latest Ver.: Ver.1.00
- Released: Sep 05, 2025
Data Flash Library Type04 for RL78 Family
- Latest Ver.: Ver.3.00
- Released: Feb 05, 2024
Note: The LLVM compiler version was added to the package.
Package for the EEPROM Emulation Library Pack02 for the RL78 Family
- Latest Ver.: Ver.3.00
- Released: May 20, 2024
Note: The LLVM compiler version was added to the package.
Package for the EEPROM Emulation Library Pack01 for the RL78 Family, the EEPROM Emulation Library T01 for the RL78 Family
- Latest Ver.: Ver.2.10
- Released: Jan 22, 2018
Note: This package is the revised edition of the following package, and the package name was changed.
- Package for the EEPROM Emulation Library Pack01 for the RL78 Family
Renesas Flash Sample Program Type01 for RL78/G15 Group and RL78/G16 Group
- Latest Ver.: Ver.1.21
- Released: Jan 20, 2026
Renesas Flash Driver RL78 Type 01 for RL78/G2x Group
- Latest Ver.: Ver.1.21
- Released: Dec 05, 2025
EEPROM Emulation Software RL78 Type 01 for RL78/G2x Group
- Latest Ver.: Ver.1.21
- Released: Dec 05, 2025
Renesas Flash Driver RL78 Type 02 for RL78/F23 and RL78/F24
- Latest Ver.: Ver.1.01
- Released: Dec 05, 2025
EEPROM Emulation Software RL78 Type02 for RL78/F23 and RL78/F24 Group
- Latest Ver.: Ver.1.01
- Released: Dec 05, 2025
Renesas Flash Driver RL78 Type 03 for RL78/F22 and RL78/F25
- Latest Ver.: Ver.1.00
- Released: Aug 05, 2024
EEPROM Emulation Software RL78 Type03 for RL78/F22 and RL78/F25 Group
- Latest Ver.: Ver.1.00
- Released: Sep 05, 2024
Details of upgrade (See Tool News)
Target Devices
Design & Development
Videos & Training
This video introduces how to reprogram the RL78/G2x data flash memory using the Renesas Flash Driver RL78 Type 01 Smart Configurator Version on e² studio.
Additional Details
Distribution Method
| Target Device Family | Distribution Method | Software name described in the download list |
|---|---|---|
| RL78/x1x | Download | Flash Self Programming Library Note1, 2 Renesas Flash Sample Program Type01 Note3 |
| RL78/x2x | Design & Development | Renesas Flash Driver RL78 Type01 Renesas Flash Driver RL78 Type02 Renesas Flash Driver RL78 Type11 Renesas Flash Driver RL78 Type03 Note4 |
| 78K (78K0R) | Contact your local Renesas Electronics marketing office or distributor when wishing to use. | - |
| RX | Application notes and sample codes for RX family related to flash programming are available. Please visit the Application Notes & Sample Code of the Documentation tab on the RX family product page. | - |
Notes:
- In the User's Manual (Hardware) for some RL78 MCUs or the User's Manual for some Flash Libraries for the RL78 family, the self RAM areas used in common for all flash libraries may be shown. However, for the latest information, please refer to the "RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語)".
- Because the self RAM areas are used as the work area for the library, using these areas for the user program is prohibited. For the latest information, please refer to the "RL78 Family Self RAM list of Flash Self Programming Library Rev.3.05 (PDF | English, 日本語)".
- Renesas Flash Sample Program Type01 for RL78/G15 group and RL78/G16 group can be downloaded from [Design & Development].
- Refer to Renesas Flash Driver and EEPROM Emulation Software Target MCU List for RL78 (PDF | English, 日本語) for Renesas Flash Driver and EEPROM Emulation Software target MCUs.
Target Devices
- RL78 Family
- 78K Family (78K0R)
Support
Support Communities
- Data over write by Data Flash Library Type 04 at 0xFAF00H for R5F100GJ
Hello, I am using Data Flash Library Type 04 for data storing in internal flash. I am using R5F100GJ micro controller and CS+ as IDE. When I called the PFDL_Open() function, It overwrite the data from 0xFAF00H memory location. as per application note, we have to allocate self RAM ...
Jun 5, 2022 - Data Flash Library type04 Execution Problem
Good evening to all, I am Using RL78/G14 micro controller with Cubesuite+ as IDE for my application I am trying to perform the read, write and erase operation in Data Flash Memory using the data flash library type04. After build operation there are two errors exist 1. Undefined ...
May 27, 2014 - data flash library for rl78f13
how to use data flash library to write data in particular address for RL78F13 IN CS+ ide
Oct 18, 2023
Knowledge Base
- Error Message E0562351 "Section ".bss" cannot be placed on the "SELFRAM area" appears when Data Flash Library is set to "Used" with the Code Generator for RL78 in e² studio
The following error message is displayed if you run a build with Data Flash Library set to "Used" when using the Code Generator for RL78. E0562351:Section ".bss" cannot be placed on the "SELFRAM area". In this case, set None for [RAM area without section] after selecting [Settings], [Tool Settings ...
Jul 26, 2019 - What is data value of code and data flash memory after erasure in MCUs?
The data value of the code flash memory and data flash memory after erasure is FFH.
Dec 20, 2013 - Is it possible to read data flash memory of RL78 without using a command?
Yes, it is possible.Data can be directly read by CPU commands by following the procedure below to make initial settings for this purpose. Write 1 to bit 0 (DFLEN) of the data flash control register (DFLCTL). Wait for the setup time (*) by using, for example, a software timer.*The ...
Dec 20, 2013