Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

How to Find the Version Number in CS+

CS+

To check the version number, follow the procedure below.

[CS+ for CC Common Program] or [CS+ for CA,CX Common Program]

  1. Start "CS+ for CC" or "CS+ for CA,CX."
  2. From the Help menu, select the About command.
  3. In the version information dialog box which is then displayed, check the version number of "CS+ for CC" or "CS+ for CA,CX."

Although the words "Common Program" are not displayed, the version number shown is that of the common program.

[CubeSuite+ Common Program V1.00.00 through V1.03.00, and V2.00.00 through V2.02.01]

  1. Start CubeSuite+.
  2. From the Help menu, select the About command.
  3. In the version information dialog box which is then displayed, check the version number of CubeSuite+.

Although the words "Common Program" are not displayed, the version number shown is that of the common program.

[Update Manager]

  1. Start the Update Manager.
  2. The version information of the Update Manager appears on the bottom left of the screen.

[Components]

  1. Open "Programs and Features" from the Windows Control Panel.
  2. Check the version number of the component of interest in the program list.

The version number is represented in a form such as V2.00.0191. Ignore the last two digits displayed, e.g. 91 in this case.