Applied Filters:
Evaluation Boards & Kits
ISLAVSEVAL1Z Active
USB to AVSBus™ Adapter
The USB to AVSBus Adapter (often referred to as a "dongle") is used to connect a demonstration board with an AVSBus interface to a PC. The USB to AVSBus adapter is powered from the USB output of the host PC. The USB interface utilizes the USB Mini format, and the output uses a standard 2-row,... Read More
Recommended Documents: