Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Description

The H8/3035 Group is supported only for customers who have already adopted these products. The RL78/G14 Group is recommended for new designs.

Part NumberStatusSamplesStockPackageLVD or PVD
HD6433035FObsoleteN/AOut of StockPackageNo

Knowledge Base

  1. How to fix 1 bit misalignment using synchronous mode and clock SCI?

    The serial interface of the H8 family and the H8S family is divided into a transmit part and a receive part structurally to be used for both asynchronous and functions. The transmit part and the receive part can be operated individually. When in synchronous transmit/receive data, each part ...

    Mar 31, 2009
  2. Why does an error occurs in asynchronous mode when starting RxD pin?

    For the serial interface in the H8 and H8S family, when a receive pin (a RxD pin) is low, start the receive operation to receive a break signal at the time the low pin was detected. Next, a framing error occurs when the serial interface could not detect the STOP ...

    Mar 31, 2009
  3. How to properly set up A/D converter?

    Depending on the operating frequency and the setting value that you are using, it can be possible to setup the conversion time, which is lower than the minimum conversion time of electrical characteristics, but in that case, accurate conversion result will not be guaranteed. All the A/D converters ...

    Mar 31, 2009
View All Results from Knowledge Base (5)