Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Features

Description

This product is obsolete.
Part NumberStatusSamplesStockPackageLead Count (#)Temp. GradePb (Lead) FreeCarrier Type
74ALVCHR16500PAObsoleteN/AOut of StockTSSOP56#CNoTube
74ALVCHR16500PA8ObsoleteN/AOut of StockTSSOP56#CNoReel
74ALVCHR16500PFObsoleteN/AOut of StockTVSOP56#CNoTube
74ALVCHR16500PF8ObsoleteN/AOut of StockTVSOP56#CNoReel
74ALVCHR16500PVObsoleteN/AOut of StockSSOP56#CNoTube
74ALVCHR16500PV8ObsoleteN/AOut of StockSSOP56#CNoReel
ALVCHR16500UObsoleteN/AOut of StockWAFER0CYesWafer