Skip to main content
Renesas Electronics Corporation

Description

The SDK-PLC-EU-A and SDK-PLC-EU-B (CENELEC B band) kits include 4 complete PLC nodes, E8a emulator, sniffer, and more. Please confirm with PLC regulations in your use region and execute the necessary procedures before it used.

Features

  • Includes 4 complete PLC nodes
  • Includes E8a emulator
  • Includes Renesas Ubiquitous Network Layer for Metering Applications evaluation version
  • Includes example SW /adaptable to particular evaluation environments & requirements
  • Includes sniffer
  • Expandable by single PLC nodes EVB08-EU-A (-B for CENELEC B band)
  • Comprehensive documentation

Applications

Part NumberStatusStockDescription
SDK-PLC-EU-AObsoleteOut of Stock
SDK-PLC-EU-BObsoleteOut of StockCENELEC B band

Knowledge Base

  1. What to do when I get an error on ID code and can't continue programming?

    The M16C Flash Starter always requires an ID code. You always need to enter an ID code to be able to program a blank Flash memory. The ID code can be any value for a blank Flash memory but you cannot leave it blank.

    Feb 14, 2006
  2. What will be written in the ID code area without setting the value?

    When programming the on-chip Flash memory without setting a value in the ID code area, the M16C Flash Starter will set "FF FF FF FF FF FF FF" in the ID code area. Therefore, the next time you reprogram the Flash memory, input [all "FFh"] to verify the ID ...

    Feb 14, 2008
  3. What is the matter why can't I program the memory using "00h" as ID code?

    ... the previous programming session. You should know this ID prior to programming the device otherwise you cannot re-program the device. (The ID code can be any value for a blank Flash memory.) Please refer to M16C Flash Starter User's Manual, Section 4.1 About the ID Check for ...

    Feb 14, 2008
View All Results from Knowledge Base (5)