Skip to main content
Renesas Electronics Corporation

Description

The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by giving the user a simple platform on which code can be run only minutes from opening box. It can also prove an invaluable tool in development by providing a useful test platform for code already debugged using one of our more powerful emulation tools.

Applications

Type Title Date
Manual - Development Tools PDF 665 KB 日本語
Tool News - Notification PDF 153 KB 日本語
Tool News - Note PDF 237 KB 日本語
Application Note PDF 357 KB 日本語
AI-generated Summary: The document explains how to manage sub-projects in CubeSuite+ by deleting unused ones from the Project Tree to streamline the build process. It details changing and setting properties of the debug tool, specifically the RX E1(JTAG), including clock frequency and power supply settings. Instructions cover building the project, starting the E1 emulator, handling warning messages related to operating frequency, and executing the program after download.
Application Note PDF 507 KB
AI-generated Summary: The document guides users through importing the RX630 Renesas Starter Kit sample code into the e2studio IDE using the GNU RX Compiler. It instructs selecting the Workbench icon, importing existing projects into the workspace, browsing to the specified directory, and ensuring the project copies into the workspace. These steps enable loading the sample project for development.
Application Note PDF 244 KB
PCB Design Files
Log in to Download ZIP 2.77 MB 日本語
Application Note PDF 61 KB 日本語
Manual - Development Tools PDF 543 KB
Manual - Development Tools PDF 833 KB
Manual - Development Tools PDF 867 KB 日本語
Manual - Development Tools PDF 1.17 MB 日本語
Manual - Development Tools PDF 92 KB
13 items

Software & Tools

Software Downloads

Type Title Date
Software & Tools - Evaluation Software
Log in to Download ZIP 37.73 MB 日本語
Upgrade - Debugger
Log in to Download ZIP 110.84 MB 日本語
Software & Tools - Other
Log in to Download ZIP 315.61 MB
Software & Tools - Other
Log in to Download ZIP 486.08 MB
Software & Tools - Evaluation Software
Log in to Download ZIP 122.90 MB 日本語
5 items

Sample Code

Sample Code

Filters
Type Title Date Date
Sample Code
Log in to Download ZIP 8.33 MB 日本語 IDE: CS+
Sample Code
Log in to Download ZIP 7.44 MB 日本語 IDE: e2 studio
Sample Code
Log in to Download ZIP 18.56 MB IDE: e2 studio
Sample Code
Log in to Download ZIP 9.86 MB 日本語 IDE: HEW
4 items
Part NumberStatusStockBudgetary Price (USD)DescriptionDebugger supplied
R0K505630S900BEObsoleteOut of Stock1u | $164.71Renesas Starter Kit for RX630None

Support Communities

  1. RX630 I2C BBSY bit always busy

    Hi, I've used the example code from the RX630 Starter Kit (an_r01an1242eg0100_rx630_rsk) for I2C Master, and i find that when i run or step through the code, it always seems to get hung on the following line of code in the Write_EEPROM_Master code: / ...

    Dec 11, 2019
  2. RX630 error messages at debug

    ... have not been able to get the RIIC0 working. Seems the BBSY flag is stuck on high. I have been using example code from a RX630 starter kit. The code breaks when i invoke the Write_I2C_Master routine in that i don't get any outright errors, it's ...

    Dec 1, 2019
  3. Syntax error sometimes with IO port pin assignments

    Hi, Not sure if this question should be under RX forums or here. I'm seeing errors in the e2 studio IDE regarding assignment of some IO port pins, but not all. For example: If i write: PORT6.PDR.BIT.B2 = 1; this is deemed OK by the editor / ...

    Dec 5, 2019