Overview
The Renesas Starter Kit for R8C/23 is intended as a user-friendly introductory and evaluation tool for the R8C/23 microcontroller. The board provides a useful platform for evaluating the Renesas suite of development tools for coding and debugging, using High-performance Embedded Workshop as well as programming the device using E8a emulator and/or Flash Development Toolkit. The Renesas Starter Kit for R8C/23 may be connected to the host PC using a simple RS232 serial connection (not normally fitted) or via the included USB E8a on chip debugging interface.
The purpose of the board is to enable the user to evaluate the capabilities of the device and its peripherals by providing a simple platform on which code can be run within minutes of opening the box. It can also prove to be an invaluable tool in development by offering a useful test platform for code that has already been debugged using one of our more powerful emulation tools.
Notes
Evaluation versions differ from their full-versions in functionality and performance. And technical support services are NOT available.
Learn More (Evaluation Software Tools)
Sample & Buy