Skip to main content
Renesas Electronics Corporation

Overview

The R0KZC000000002R converts the 14-pin connector of the E8a (or the E8) emulator to the 10-pin connector. When using this product, make sure that the pin assignment of the target system is the same as the following connector pin assignment. It can be used only when the pin assignment of the 10-pin connector-side is the same.

Products in the Design

Sample & Buy

E8a/E8 14PIN-10PIN Convert Board

E8a/E8-14PIN-10PIN-Convert-Board

Obsolete

Support

Support Communities

  1. 14pin_10pin convert board

    Hello friendsi have E8a demodulator. and a bourd with M16C/tiny. i want to program my board but on board there is 10 pin and the conector of E8a has 14 pin.i think i need 14-10pin convert board.could you please help me to build this convert ...

    Jul 13, 2011