Skip to main content

Renesas Blog

Successful Debugging Requires Bridging the Hardware-Software Gap Blog

Successful Debugging Requires Bridging the Hardware-Software Gap

Debugging is an important part of embedded design; one that requires bridging the hardware/software gap.

RX - The Road Ahead!

RX - The Road Ahead!

For the RX MCU family, consumer and industrial applications will continue to be our primary focus in the next few years. We will also focus on IoT-related applications in these two areas.

The Art of Networking (Series 7): TSN in a Virtualized Environment

The Art of Networking (Series 7): TSN in a Virtualized Environment

Here, we show solutions for Precision Time Protocol (PTP) time distribution to virtualized OS with the help of hardware-assisted virtualization (Renesas R-Switch2) to solve challenges quickly.

Achieving a root of trust with secure boot in automotive RH850 and R-Car devices – Part 2

Achieving a Root of Trust with Secure Boot in Automotive RH850 and R-Car Devices – Part 2

There are 2 types of security IP on RH850 automotive MCUs, ICU-S and ICU-M. In this blog article, part 2 in a three-part series, we introduce how secure boot is realized on both types of devices.

Water level measurement solution blog

Realizing a Low-Cost Water Level Measurement Solution Using the RX130’s Capacitive Touch Key

Introducing a reference design demo that can measure the amount of remaining liquid with the RX130 MCU, using its built-in Capacitive Touch Sensor Unit (CTSU) and copper electrodes.

Use the Latest Technology in Your Next BLDC Motor Control Design

Use the Latest Technology in Your Next BLDC Motor Control Design

Learn about Renesas’ BLDC Traction Motor Drive solution that is built around two dedicated motor control devices for the perfect combination of processing speed and power efficiency.

The Art of Networking: MACsec and CANsec – Layer 2 Security for High Performance Networks

The Art of Networking (Series 6): MACsec and CANsec – Layer 2 Security for High Performance Networks

In this blog, we will explain security acceleration methods that are being standardized for CAN and Ethernet to improve the security performance and offload tasks to hardware.

Seamlessly Switch to a 32-Bit RX Family MCU

To Seamlessly Switch to a 32-Bit RX Family MCU

Renesas has prepared a “Migration Guide” and “Points of Differences” to support replacement from Renesas legacy MCU products to the RX 32-bit MCU family, as well as between the RX family itself.

Achieve Ultra-Lower Designs Using the RA2E1 MCU and Flexible Software Package (FSP).

Achieve Ultra-Lower Designs Using the RA2E1 MCU and FSP

Quickly develop a low power data logger application on the RA2E1 32-bit MCU using its “Snooze” mode for significant power savings, Flexible Software Package (FSP) and Fast Prototyping Board (FPB).

Address the challenges of network-connected equipment by using 32-bit RX66N MCUs.

Would You Like to Address the Challenges of Network-Connected Equipment by Using 32-Bit RX66N MCUs?

Introducing the RX66N 32-bit MCU that realizes real-time performance and firmware updates required for network-connected equipment such as smart meters and HVAC controllers.