To check the version number, follow the procedure below.
[CS+ for CC Common Program] or [CS+ for CA,CX Common Program]
- Start "CS+ for CC" or "CS+ for CA,CX."
- From the Help menu, select the About command.
- In the version information dialog box which is then displayed, check the version number of "CS+ for CC" or "CS+ for CA,CX."
Although the words "Common Program" are not displayed, the version number shown is that of the common program.
[CubeSuite+ Common Program V1.00.00 through V1.03.00, and V2.00.00 through V2.02.01]
- Start CubeSuite+.
- From the Help menu, select the About command.
- In the version information dialog box which is then displayed, check the version number of CubeSuite+.
Although the words "Common Program" are not displayed, the version number shown is that of the common program.
[Update Manager]
- Start the Update Manager.
- The version information of the Update Manager appears on the bottom left of the screen.
[Components]
- Open "Programs and Features" from the Windows Control Panel.
- Check the version number of the component of interest in the program list.
The version number is represented in a form such as V2.00.0191. Ignore the last two digits displayed, e.g. 91 in this case.
Support
Support Communities
Get quick technical support online from Renesas Engineering Community technical staff.
Knowledge Base
Browse our knowledge base for helpful articles, FAQs, and other useful resources.