The Importance of Reference Documentation for Consumers and Engineers
In this blog, we examine the differences in documentation needs between consumer products and engineering products.
In this blog, we examine the differences in documentation needs between consumer products and engineering products.
Renesas is working on the development of a solution that allows developers to develop applications without considering device configuration.
Renesas' co-simulation environment for multi-devices enables software development with inter-device communication without actual devices for early development of E/E architectures.
This blog series introduces standardizing the design of sensing equipment using the RX23E-A MCU’s built-in high-precision delta-sigma ADC. Blog 1 highlights the standardization between models of a product.
This blog explains how Renesas views the evolution of the automotive industry and builds its business strategy.
How we can use the Data Operating Circuit and the Data Transfer Controller to create complete, autonomous subsystems that can make simple decisions based on measured data without CPU intervention.
Multiplexed Register Clock Driver (MRCD) and Multiplexed Data Buffer (MDB) components allow DDR5 memory modules to deliver significantly higher bandwidth for memory sub-systems in next-generation servers.
Renesas offers a solution that adapts well in remote locations where there is no Wi-Fi or Bluetooth LE access, only a cellular radio using CAT-M1; the inclusion of solar energy harvesting into the design allows for long-term battery life.
A waterproof self-capacitance solution, using a new feature of CTSU2SL within the latest RX140 MCU, is suitable for implementing capacitive touch keys in space-constrained, wet-area applications.