Download (D4000107)

Issue Date : Oct.05.16

Category : Evaluation Software

[Evaluation Software] CS+ for CC V4.01.00 (Single Download)

Description

For the CS+, see Products Information.
You can download an installer of the evaluation product from this page.
If you download it as seven files, see "Multipart Download" from here.

CS+ is not generally promoted to the U.S. and European customers. Customers in the U.S. and Europe who are interested in CS+ are requested to contact our regional marketing departments for details.

Supported MCUs

  • RH850 Family
  • RX Family
  • RL78 Family

For the supported MCUs' part numbers, please refer to the data sheet.

Main included modules

Category Product Name
Main program group CS+ for CC common program V4.01.00
Compiler RH850 Compiler CC-RH V1.04.00
RX Compiler CC-RX V2.05.00
RL78 Compiler CC-RL V1.03.00
Device Information CS+ Device Information for RH850 V4.00.02
CS+ Device Information for RX V1.12.00
CS+ Device Information for RL78 V4.00.02
Code Generator Code Generator Common (CS+ for CC) V1.09.00
CS+ Code Generator for RX V1.11.00
CS+ Code Generator for RL78 V2.12.00
Quick and Effective tool solution - QE QE V1.01.00

The included modules may be upgraded individually. After installing this product, update the modules to the latest version with the update manager.

Caution on updating CC-RX and CC-RH

The CC-RX and CC-RH compiler have the following two editions from CS+ V3.02.00.
- standard edition
- professional edition

Start a License Manager to make the license of " RX License Pack 2 Professional(CC-RX)" and " RH850 License Pack 1 Professional(CC-RH)" registered at present enable.

Notes

  • Limitation

    For details, please refer to Evaluation Version Software Information before downloading!! Depending on the type of MCU, the evaluation version is subject to the following limitations:
    Target MCU Limitation
    RH850 Family Expires 60 days after the first build following the initial installation of the evaluation version.
    Fully functional during the evaluation period.
    The size of linkable object is limited to 256 KB and professional edition function isn't supported on or after the 61st day.
    RX Family Expires 60 days after the first build following the initial installation of the evaluation version.
    Fully functional during the evaluation period.
    The size of linkable object is limited to 128 KB and professional edition function isn't supported on or after the 61st day.
    RL78 Family Expires 60 days after the first build following the initial installation of the evaluation version.
    Fully functional during the evaluation period.
    The size of linkable object is limited to 64 KB and professional edition function isn't supported on or after the 61st day.

  • Installation

    If you install the free evaluation version downloaded from the Internet, make sure that your host machine is connected to the network before installing the program. If you install the program on a host machine that is not connected to the network, first go to the Microsoft Download Center and install the Microsoft .NET Framework 4.5.2 before installing CS+.

  • Operational Environment

    Host machine *1 IBM PC compatible machine
    OS *2 Windows® 7
    Windows Vista®
    Windows® 8.1
    Windows® 10
    Memory capacity 2 GB or more recommended.
    Minimum requirement is 1 GB or more
    (Windows 10 and any 64-bit Windows requires 2 GB or more)
    Available hard disk space 1 GB or more
    Display 1024 x 768 or higher resolution,
    65,536 or more colors
    I/O device DVD drive
    Others Mouse or compatible pointing device,
    .NET Framework 4.5.2,
    Microsoft Visual C++ 2010 SP1 runtime library,
    Internet Explorer 9 or later

    *1.IBM is registered trademarks of International Business Machines Corporation.

    *2.Windows® is registered trademarks of Microsoft Corporation in the U.S. and other countries.

    *All other company names and product names are trademarks or registered trademarks of corresponding companies.


  • Other Notes

    1. The folder or file name which comprised of ASCII character-code only can be used.
    2. A period (.), indicating an extension, can be used only once in a file name.
    3. Assign the installation path to the internal drive.
    4. No more than 1 upper directory can be specified using "...".
    5. When you install CS+ V3.00.00 or later, CubeSuite+ V2.xx.xx is uninstalled.

Download

Product Name File Name File Size Download Link
[Evaluation Software] CS+ for CC V4.01.00 (Single Download) CSPlus_CC_Package_V40100.exe 472.79 MByte