Overview
Description
Embedded Target supports the new device RL78/L23.
We offer the above tool for co-simulation between the CS+/e² studio integrated development environment from Renesas interlinked with MATLAB® and Simulink® from the MathWorks, Inc. Among other things, this will support the validation of algorithms and model-based development by customers. For more information of this tool related to using evaluation version or purchasing commercial version, please refer to the release information.
Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.
Features
- Generation of code for verifying algorithms from Simulink models
- Automatic generation of Processor in the Loop Simulation (PILS) environments
- Supported MCU families: RA, RX, RL78
- What Customers Will be able to Do: Verify the functionality of code for target devices/Measure the performance of code for target devices
- Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
- Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
- Learn More
Release Information
Latest Ver: V6.08.00.
Released: Mar 21, 2025
A license key is required to use the Embedded Target. Please check contents in below before using this tool.
For customer who consider commercial version of the Embedded Target
The Embedded Target is a tool that works with multiple software tools in tandem. Therefore, before purchasing commercial version license of this tool, we recommend that you check operating environments of the Embedded Target carefully and try the free evaluation version (limited 2 months usage) on your development environment first to check if it works properly.
This tool may not work properly under the following conditions.
- MATLAB® versions are not supported by this product.
- Specifications of Renesas MCU (such as small ROM/RAM size)
- When a size of generated codes, which are affected size and complexity of the Simulink® model, is larger than ROM size of the MCU.
- Inability to communicate due to network security settings, etc.
Again, please check operating environments of the Embedded Target carefully.
Embedded Target Evaluation Version Information
We will guide you through technical support.
Please refer to the following procedure.
- Access technical support on the Renesas Web site.
- Click on [LOG IN] and log in to the site with your ID which has been registered with My Renesas.
- Click on [SUBMIT A TICKET] in the upper right of the screen.
- Issue a new ticket by referring to the table and examples of entry which are shown to the right side.
Title: Request a License Key for Evaluation version of the Embedded Target
Inquiry Product Category: Microcontrollers & Microprocessors
MCU Product Family: Renesas MCU (a device from the RA, RL78, or RX family) that is usable with Embedded Target
Microcontrollers & Microprocessors: Technical Inquiry of MCU Tools
Tool Name: Embedded Target for (the device you will be using)
Description: Describe the purpose for use and field of application for Embedded Target and your previous experience in using model-based development environments including MATLAB®.
Embedded Target Evaluation Version Information
Please check the "Software License Agreement" and "Licenses for Purchasing Commercial Version of the Embedded Target" in the detailed information, and contact your dealer, our sales representative, or our technical support.
Note: MATLAB®, Simulink® are registered trademarks of The MathWorks, Inc.
Target Devices
Target Devices
Note
- The Embedded Target may not work properly with certain ROM/RAM size of a device and/or size and complexity of a model.
We recommend tying the evaluation edition on your development environment first to check if it works properly. - When using Embedded Target with an RA family device, an emulator and an actual device are required to perform PILS (Processor In the Loop Simulation). In addition, additional settings are required to match the FSP version and GCC version in use. For more information, refer to FAQ in below.
FAQ: Project cannot be generated when using RA family in Embedded Target. (Embedded Target error code E300) - The FSP installer for RA family is available on GitHub.
See All Versions(GitHub)
Design & Development
Support
Support Communities
Videos & Training
This video will introduce a useful software tool: Embedded Target. It can help developers reduce both testing time and costs in model-based development. Embedded Target can create an automatically configured model for the PILS environment. Next it generates a Renesas IDE project for PILS. Finally, model verification is performed by checking the execution time on an MCU or simulator.
Chapter's Title
00:00 Introduction
00:19 About Model-Based Development
03:13 About Embedded Target
Additional Details
Functionality
- Generation of code for verifying algorithms from Simulink models
- Automatic generation of Processor in the Loop Simulation (PILS) environments
- Supported MCU families: RA, RL78, RX
What Customers Will be able to Do
- Verify the functionality of code for target devices and
- Measure the performance of code for target devices
Other Benefits to Customers
- Environments for evaluation through PILS are easy to construct from Model in the Loop Simulation (MILS) environments.
- Evaluation by comparing the results of MILS and PILS (back-to-back testing) is simple and reliable.
Software License Agreement
Licenses | Software License Agreement |
---|---|
Node-Locked License | Software License Agreement (for Node Locked License) (PDF | English, 日本語) |
Licenses for Purchasing Commercial Version of the Embedded Target
Give the part number from the list below to the distributor.
Embedded Target for RA family Node Locked License | ||
---|---|---|
Period | Number of Licenses | Part Number |
annual | 1 | RTCRA0000ET00WNJ |
5 | RTCRA0000ET00WNJL5 | |
10 | RTCRA0000ET00WNJLA |
Embedded Target for RL78 family Node Locked License | ||
---|---|---|
Period | Number of Licenses | Part Number |
annual | 1 | RTCRL7800ET00WNJ |
5 | RTCRL7800ET00WNJL5 | |
10 | RTCRL7800ET00WNJLA |
Embedded Target for RX family Node Locked License | ||
---|---|---|
Period | Number of Licenses | Part Number |
annual | 1 | RTCRX0000ET00WNJ |
5 | RTCRX0000ET00WNJL5 | |
10 | RTCRX0000ET00WNJLA |
Learn More
For more information related with the Embedded Target commercial version or evaluation version, please contact a Renesas Electronics distributor, sales representative in your area or Technical Support on Renesas Web.