Basic Library
Digital I/O
Analog I/O
Advanced I/O
Time
Math
Trigonometry
Random Numbers
Bits and Bytes
Interrupts
Serial Comm.
Standard Library
Ethernet
Servo Motor
Stepping Motor
Character LCD
SPI
I2C (Wire)
SD Card
SD (File Operations)
Periodic Operation
Clock (RTC)
PPG (Pulse Generator)
WiFiEsp
ICS (Serial Servo)
FreeRTOS Tips
Real-Time Clock (RTC)
This library allows users to get a clock after setting the year, month, date, hour, minutes, and seconds. To use this library, create an instance like "RTC rtc" and describe #include <RTC.h>
begin
- Description
- Initialize RTC.
- Syntax
- bool rtc.begin()
- Parameters
- None
- Returns
- True or False
end
- Description
- Stop RTC.
- Syntax
- bool rtc.end()
- Parameters
- None
- Returns
- True or False
setDateTime
- Description
- Set a start time.
- Syntax
- bool rtc.setDateTime(int year, int mon, int day, int hour, int min, int sec, int week)
- Parameters
- year: Year
mon: Month
day: Day
hour: Hour
min: Minute
sec: Second
week: Use the following parameters.
RTC_WEEK_SUNDAY
RTC_WEEK_MONDAY
RTC_WEEK_TUESDAY
RTC_WEEK_WEDNESDAY
RTC_WEEK_THURSDAY
RTC_WEEK_FRIDAY
RTC_WEEK_SATURDAY - Returns
- True or False
getDateTime
- Description
- Get a current time.
- Syntax
- bool rtc.getDateTime(int &year, int &mon, int &day, int &hour, int &min, int &sec, int &week)
- Parameters
- Variables are the same as setDateTime.
- Returns
- True or False
attachAlarmHandler
- Description
- Register a function when an alarm occurs.
- Syntax
- void rtc.attachAlarmHandler(void (*function)(void))
- Parameters
- function: Function to be called when an alarm occurs
- Returns
- None
setAlarmTime
- Description
- Set an alarm time.
- Syntax
- bool rtc.setAlarmTime (int hour, int min, int week_flag)
- Parameters
- hour: Hour
min: Minute
week_flag: Use the following week parameters:
RTC_ALARM_SUNDAY
RTC_ALARM_MONDAY
RTC_ALARM_TUESDAY
RTC_ALARM_WEDNESDAY
RTC_ALARM_THURSDAY
RTC_ALARM_FRIDAY
RTC_ALARM_SATURDAY
RTC_ALARM_EVERYDAY - Returns
- True or False
alarmOn
- Description
- Set alarm on.
- Syntax
- rtc.alarmOn()
- Parameters
- None
- Returns
- None
alarmOff
- Description
- Set alarm off
- Syntax
- rtc.alarmOff()
- Parameters
- None
- Returns
- None
Sample Program
This example shows a program for setting a time and alarm. Time and alarm notification is output by flashing LED.
#include <Arduino.h>
#include <RTC.h>
RTC rtc;
int g_year = 2019;
int g_mon = 1;
int g_day = 30;
int g_hour = 9;
int g_min = 20;
int g_sec = 50;
int g_week = RTC_WEEK_WEDNESDAY;
void alarm_handler();
void setup()
{
Serial.begin(9600);
pinMode(PIN_LED1, OUTPUT); // led for alarm
digitalWrite(PIN_LED1, LOW); //turn off
rtc.begin();
rtc.setDateTime(g_year, g_mon, g_day, g_hour, g_min, g_sec, g_week);
rtc.attachAlarmHandler(alarm_handler);
rtc.setAlarmTime(g_hour, g_min + 1, g_week);
rtc.alarmOn();
}
void loop()
{
rtc.getDateTime(g_year, g_mon, g_day, g_hour, g_min, g_sec, g_week);
Serial.print(g_year, DEC);Serial.print("/");
Serial.print(g_mon, DEC); Serial.print("/");
Serial.print(g_day, DEC); Serial.print(" ");
Serial.print(g_hour, DEC); Serial.print(":");
Serial.print(g_min, DEC); Serial.print(":");
Serial.println(g_sec, DEC);
delay(500);
}
void alarm_handler()
{
digitalWrite(PIN_LED1, HIGH);// led for alarm
}
Support
Support Communities
Get quick technical support online from Renesas Engineering Community technical staff.
Knowledge Base
Browse our knowledge base for helpful articles, FAQs, and other useful resources.