Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

VersaClock 3 / LP Software Download and Installation Guide

This page contains the required files and installation instructions for the latest version of Renesas's VersaClock software to be used with the VersaClock 3 and VersaClock LP family of programmable clocks. Please follow the instructions below to install the software. For additional support, customers may submit a technical support request using this link.

Notice: VersaClock 5 devices use Renesas’s Timing CommanderTM platform. Please visit the Timing Commander page to download software for VersaClock 5 devices.

File Downloads

Please choose the download package that corresponds to your operating system.
*Note: VersaClock 3/LP is not supported on Windows 7 Enterprise Edition at this time
*Note: Supports VersaClock 3 and LP only. VersaClock 5 uses Timing CommanderTM

OPERATING SYSTEM
 
Windows XP 32-bitDownload
Windows XP 64-bit not supported
Windows Vista RTM & Service Pack 1 32-bitDownload
Windows Vista RTM & Service Pack 1 64-bitDownload
Windows Vista Service Pack 2 32-bitDownload
Windows Vista Service Pack 2 64-bitDownload
Windows 7 Professional Service Pack 1 32-bitDownload
Windows 7 Professional Service Pack 1 64-bitDownload
Windows 7 Enterprise Edition 32-bitnot supported
Windows 7 Enterprise Edition 64-bitnot supported

 


 

Installation Guide

  1. Files summary of download package (download from above)
  2. Supported operating systems
  3. Prerequisites included in this package
  4. Preparing to install
  5. Install the VersaClock software
  6. If applicable, install drivers for the VersaClock Evaluation Board

 

1.  Files Summary of Download Package

READ_ME.txt Installation Guide
Install_IdtSqlServer.bat Installs SQL Server 2008 (Renesas)
SQLEXPR_x86_ENU_SP3.exe SQL Server 2008 Installer, invoked by Install_IdtSqlServer.bat
VersaClock.msi   VersaClock Installer
VersaClock User GuideFor reference
FTDI Driver Installation GuideFor reference

 

2. Supported Operating Systems

 

  • Windows XP SP2, SP3  (32-bit only)
  • Windows Vista RTM, SP1, SP2 (32- and 64-bit)
  • Windows 7 Professional RTM, SP1 (32- and 64-bit)

*Note: VersaClock is not supported on Windows 7 Enterprise Edition at this time
 

3. Prerequisites Included In This Package

  • Prerequisite for all systems: SQL Server 2008 (SP3)
  • Prerequisites for Windows XP and Windows Vista: Windows Installer 4.5 (except: already installed on Vista SP2) and .NET Framework 3.5
  • Prerequisites for Windows 7: None. Windows Installer 4.5 and .NET Framework 3.5 are already installed.
     

4. Preparing to Install

  1. First, unzip or copy the installation files into a temporary folder such as your desktop. 
     
  2. Remove any earlier instances of Renesas SQL Server. (To do this, you must be a local administrator with permission to log on as a service.) Depending on your installation, it may be an instance of SQL Server 2005 or SQL Server 2008.

    Using Control Panel/Uninstall, open the list of installed programs and scroll down to Microsoft SQL Server. There may be one or more versions identified by year (e.g. 2005, 2008, etc.) but only one will be a Renesas instance. Beginning with the oldest, begin to uninstall it. The uninstall dialog will ask for the instance you want to remove, and should offer an instance with Renesas in the name. If it doesn’t, cancel and proceed to the next later version. If it does, go ahead and remove it. If Renesas is the only instance, then also remove the associated components at the same time. Both options will be on the same dialog. 
     

    Using Control Panel/Uninstall, also uninstall Microsoft SQL Server Native Client, if present. If there is more than one version, use the version number and/or install date to remove the one associated with the SQL Server instance you just uninstalled.
     
    For more information, see How to: Uninstall an Existing Instance of SQL Server 2005 (http://msdn.microsoft.com/en-US/library/ms143412(v=sql.90).aspx).
     
  3. Install any prerequisite software required by your operating system:
     
    • For Windows XP:  If you have not already done so, update the Windows Installer (click the link to download) by executing WindowsXP-KB942288-v3-x86.exe. If you are not sure if this has already been done, do it anyway. Reinstalling won't hurt. You will be prompted to restart the machine.
       
    • For Windows Vista (except Vista SP2):  If you have not already done so, update the Windows Installer (click link to download). Execute Windows6.0-KB942288-v2-x86.msu on 32-bit systems and Windows6.0-KB942288-v2-x64.msu on 64-bit systems. If you are not sure if this has already been done, do it anyway. Reinstalling won't hurt. You will be prompted to restart the machine.
       
    • For Windows XP and Windows Vista (all versions):   If you have not already done so, install .NET Framework 3.5 (click the link to download) by executing dotnetfx35.exe. If you are not sure if this has already been done, do it anyway. Reinstalling won't hurt.
       
    • For all supported operating systems:  Install Sql Server (Renesas) by running the batch file  Install_IdtSqlServer.bat. (To do this, you must be a local administrator with permission to log on as a service.)
       

5. Install VersaClock Software

Run the VersaClock installer VersaClock.msi. Unlike earlier versions, this installs both the software and the local database.

 

6. If Applicable, Install the Drivers for the VersaClock Evaluation Board

The VersaClock Evaluation Board uses FTDI parts for USB and I2C protocols. To install the drivers, follow the instructions in the appropriate installation guide below.

For Windows XP:
  • AN_104_FTDI_Drivers_Installation_Guide_for_WindowsXP(FT_000093).pd
For Windows 7 and Vista (both 32- and 64-bit):
  • AN_119_FTDI_Drivers_Installation_Guide_for_Windows7.pdf

When asked, browse to the following folder:

  •   32-bit systems:
      C:\Program Files\Integrated Device Technology, Inc\VersaClock®  4.2\VersaClock Evaluation Board
  •   64-bit systems:
      C:\Program Files (x86)\Integrated Device Technology, Inc\VersaClock®  4.2\VersaClock Evaluation Board