Renesas Electronics Corporation

Categories: Development

This solution package includes the files and documentation needed to implement a self-capacitive touch button solution for S1 and S3 series Synergy microcontrollers (MCUs).

The self-capacitive touch button solution package provides the user with a set of calibration factors and allows for quick implementation of button-based capacitive touch solutions, with the following limitations:

  • Only self-capacitance
  • No wheel and sliders
  • Up to sixteen buttons

Features

The capacitive touch sensing unit (CTSU) driver used in this package features:

  • Reduced memory footprint and a set of calibration parameters to support simplified implementation of the driver
  • Uses the Capacitive Touch Workbench for Renesas Synergy v1.06

Release Information

This is a User Specific Release – Therefore only users who have access are able to download it.

If you are accessing this page by a URL that was shared with you and do not see the Download button, it is because the software is inaccessible for you to download.

Please contact your Renesas representative to inquire about this release and ask to be included in the access list.

Synergy Download