Skip to main content

Renesas Blog

RX72M Single-Chip Motor Control via EtherCAT Communications

RX72M Single-Chip Motor Control via EtherCAT Communications

To solve recent factory automation issues, Renesas proposes an RX72M Motor + EtherCAT single-chip solution, which realizes application processing, standard EtherCAT communication and motor control.

The RX671 Microcontroller Meets the Ever-evolving Demands of IoT Devices Blog

The New RX671 Microcontroller Meets the Ever-Evolving Demands of IoT Devices

The RX671 microcontroller with enhanced computing capabilities and function has contributed to the evolution of smart home appliances and industrial equipment.

The Art of Networking (Series 3): The Power of Virtualization Blog

The Art of Networking (Series 3): The Power of Virtualization

In this blog, we describe a proof of concept (POC) where we compare the benefit of having two virtual machines (VMs) sharing an integrated hardware switch against a software switch.

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Accelerate Your Design Process with Renesas’ Lab on the Cloud

Renesas’ Lab on the Cloud bridges the gap between ordering evaluation boards and testing in the lab by providing access to live boards in a physical lab through an online interface.

Evaluation Environment for Dual Motor Control Using the Renesas RA Family RA6T1 Group Blog

Evaluation Environment for Dual Motor Control Using the Renesas RA Family RA6T1 Group

Using two of our already commercially available motor evaluation kits, users can control dual motors simultaneously by changing the motor control parameters on the simple provided GUI.

Merits of Using the Verified Linux Package in the RZ/G Board Support Package Blog

Merits of Using the Verified Linux Package in the RZ/G Board Support Package

This blog details the benefits of the Verified Linux Package which incorporates an industrial-grade Linux Civil Infrastructure Platform Super Long-term Support kernel in the RZ/G series’ Board Support Package.

100W Power Adaptor with Power Delivery and Wireless Charging Solution Blog

Carry Fewer Chargers with the 100W Power Adaptor with Power Delivery and Wireless Charging

The 100W Power Adaptor with Power Delivery and Wireless Charging Solution eliminates the need for multiple chargers by providing simultaneous use for wireless charging, USB-C with PD and two standard USB ports.

Smart Asset Tracking Label Blog Image

Smart Asset Tracking Label: The Future of Package Tracking

Our smart asset tracking label solution is a Bluetooth Low Energy, multi-sensor solution supporting data logging, real-time inventory and environmental data monitoring to prevent record and time-stamp inventory loss and damage.

Realize OTA update using RX MCU with Bluetooth Low Energy (Bluetooth LE) wireless communication

Realize OTA Updates Using an RX MCU with Bluetooth Low Energy (Bluetooth LE) Wireless Communication

This blog introduces Renesas’ Over-the-Air (OTA) solution that uses Bluetooth Low Energy (LE) wireless technology to update the RX23W firmware from your smartphone.
CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility Blog

CPX3 – The First Powerline Solution with a PRIME 1.4 Certification Supporting Security Profiles and Backward Compatibility

The R9A06G037 Cool Phoenix 3 Powerline Modem (CPX3) has been re-certified to the PRIME Powerline standard Version 1.4 covering all security profiles as well as backward compatibility features.