Skip to main content

Renesas Blog

Experience Digital Signal Processing  with RX MCU on the Cloud!

Experience Digital Signal Processing with RX MCU on the Cloud!

This blog introduces the RX Family DSP Solution on Lab on the Cloud, where you can connect to the RX microcontroller's evaluation board online and experience DSP firsthand

Renesas Powers a New Space Race

Renesas Powers a New Space Race

This blog discusses Renesas’ high-reliability (Hi-Rel) business, what’s driving the space race for Renesas, and what lies ahead.

<style type="text/css">@media (min-width: 996px) { .col-lg-7.first_blog_p { padding-left: 50px; }} @media (max-width: 995px) { .col-lg-7.first_blog_p { padding-top: 50px; }} </style> <div class="row"> <div class="col-lg-5" style="padding: 20px 20px 0px 20px;border: 1px solid #e1e0e0; border-radius: 4px;"> <h4>Radar Transceivers: Key Components for ADAS &amp; Autonomous Driving</h4>  <ul> 	<li><a data-entity-substitution="canonical" data-entity-type="node" data-entity-uuid="d18059ba-52f0-4c58-9978-db1070c9bd

How to connect the antennas?

At mmWaves the interfaces between the radar MMIC and the antennas need to be carefully designed to avoid any degradation on the system performance. This issue of the blog will highlight some aspects that need to be considered in the design of the transitions for different antenna configurations.

Configuration Issues with the RA6 Ethernet Controller

Configuration Issues with the RA6 Ethernet Controller

Are you having issues with the Ethernet controller on the RA6 MCU family? This blog suggests that you should check the configuration of the Arm® TrustZone® boundaries and explains why.

Let's Make a Game Using a Microcontroller Blog - Part 2

Let's Make a Game Using a Microcontroller - Part 2

This blog introduces the components and circuit diagram used in the hardware design to build a falling block puzzle game with an RL78 microcontroller. The source code is also available.

Solution for debugging and profiling multiple automotive devices

Solution for debugging and profiling multiple automotive devices

We will introduce a solution that resolves problems in the development of software in an environment which requires the coordinated operation of multiple devices.

Single MCU Solution for Safety-Related Applications Using TrustZone Blog

Single MCU Solution for Safety-Related Applications Using TrustZone

Learn how RA 32-bit MCUs enable implementing a Class C application on a single microcontroller.

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

Renesas RZ/G2M Awarded Arm SystemReady IR 1.1 Certification

The Renesas RZ/G2M platform is the first RZ/MPU platform to be officially certified by Arm as compliant with SystemReady IR 1.1, a set of interoperability specifications targeting edge and IoT devices.

Power Up Your SPI Transfers

Power Up Your SPI Transfers

This blog looks at how we can automate a series of SPI transfers using the command sequencer implemented on many RA 32-bit MCU devices.

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution? Blog

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution?

Gigabit speed and its associated frequencies require sophisticated schematics and PCB design. Renesas’ Gigabit Industrial Ethernet SoM solution contains all of the needed mission-critical components.