e² studio

 

How to Use the e² studio

Various guides to the basic usage of the e² studio are available as listed in the table below. You can also view a video on how to download and install the e² studio. Watch the video. >>

Renesas MCUs Installation Building and Debugging Generating Code
RA family Renesas e² studio 2021-04 or higher User's Manual: Quick Start Guide Renesas MCU RA Family (PDF | English, 日本語) See the Web page on the Flexible Software Package (FSP) for the RA Family.
RE family Renesas e² studio 2021-07 or Higher User's Manual: Quick Start Guide Renesas MCU RE Family (PDF | English, 日本語) See the Web page on theRE Software Development Kit.
RX family e² studio Integrated Development Environment User's Manual: Getting Started Guide RX, RL78, RH850 Family Rev.1.00 (PDF | English, 日本語) RX Smart Configurator User's Guide: e² studio Rev.1.40 (PDF | English, 日本語)
RL78 family e² studio Integrated Development Environment User's Manual: Getting Started Guide RX, RL78, RH850 Family Rev.1.00 (PDF | English, 日本語) See Chapter 3 and subsequent chapters of the AP4, Applilet3 Common Operations User's Manual (PDF | English, 日本語).
RH850 family e² studio Integrated Development Environment User's Manual: Getting Started Guide RX, RL78, RH850 Family Rev.1.00 (PDF | English, 日本語)
RZ family e² studio Integrated Development Environment User's Manual: Getting Started RENESAS MCU RZ Family Rev.1.02 (PDF | English, 日本語) (Note1)
Renesas Synergy e² studio ISDE Renesas Synergy Standalone Configurator (SSC)

Note

  1. The user guides for the code-generating tools for the other groups of the RZ Family are being prepared.

Tools supported for individual MCU families

Compilers for the e² studio

Renesas MCUs Compilers
Renesas (Note1) GNU (Note2) IAR (Note3) GHS ARM (Note4)
RA family lens lens lens
RE family lens lens
RX family lens lens lens
RL78 family lens lens lens
RH850 family (Note5) lens lens
RZ family lens
Renesas Synergy™ (Note6) lens lens

lens Supported | — Not supported

Note

  1. The version numbers of Renesas compilers which can be used with the e² studio are as follows:
    • C/C++ Compiler Package (CC-RX) for RX Family: V2.00.01 and later versions
    • C Compiler Package (CC-RL) for RL78 Family: V1.01.00 and later versions
    If you have installed CC-RX or CC-RL with the above-mentioned version numbers with the CS+ IDE, you can also use them with the e² studio, i.e. you do not need to install the version without the IDE.
  2. GNU tools that include GNU compilers can be installed by selecting them with the installer of the e² studio (Internet connection is required).
    Also, the GNU tools for each family can be installed free of charge by downloading them from the GNU Web site (registration is required for the e² studio which has already been installed).
  3. Using the e² studio in debugging requires building load modules in the ELF/DWARF format. Refer to the following table "Debugging tools" for the supported emulators. IAR provides plug-ins to handle projects for IAR compilers. See here for details. >>
    Contact IAR Systems K.K. for details of the IAR Embedded Workbench, compiler products, and plug-ins for Eclipse.
    IAR Systems K.K.: http://www.iar.com/
  4. Manually need to add ARM Compiler 6 to Toolchain to use on e² studio.
  5. Only the debugging functions of the e² studio can be used with products of the RH850 family. The e² studio can be used to debug load modules in the ELF/DWARF format which were built with the IAR Embedded Workbench from IAR Systems or the MULTI IDE from Green Hills Software.
  6. Use the IAR Embedded Workbench for Renesas Synergy or the e² studio ISDE for Renesas Synergy. They can be downloaded free of charge from the following Web site.
    Renesas Synergy™ Platform >>

Debugging tools for the e² studio

Renesas MCUs Debugging tools
Renesas Simulator E2 emulator E1 emulator E2 emulator Lite E20 emulator IECUBE Segger J-Link
RA family lens lens lens
RE family lens lens lens
RX family lens lens (Note1) lens lens lens (Note2) lens
RL78 family lens lens lens lens lens
RH850 family lens (Note3) lens
RZ family lens
Renesas Synergy lens

lens Supported | — Not supported

Notes

  1. The E2 emulator is under development so that JTAG connection is supported for the current measurement.
  2. The usable functions of the E20 emulator for RX family MCUs other than those of the RX600 and RX700 series are the same as for the E1.
  3. The E2 emulator can be used with V7.0.0 and later versions of the e² studio. The usable functions are the same as for the E1.

Code generators and other useful functions for the e² studio

Renesas MCUs (Note1) Code generator Smart Utility
Family Group Smart Configurator Smart Manual Smart Browser Assistant for Optimization
RA family lens lens lens
RE family lens lens
RX family lens lens lens lens lens
RL78 family lens lens (Note2) lens lens lens
RH850 family
RZ family RZ/T lens lens lens
RZ/G lens
RZ/A1 lens lens
RZ/A2 lens lens
Renesas Synergy lens  (Note3)

lens Supported | — Support is not planned.

Notes

  1. For details of Renesas MCUs, refer to the Product Info page for the individual products.
  2. Only RL78/G23 is supported.
  3. The Synergy Software Package supports the code generator. Download the package from the Web site for Renesas Synergy.
 

QE (Quick and Effective Tool Solutions) for the e² studio

Renesas MCUs (Note1) QE for Motor QE for USB QE for BLE (Note3) QE for TCP/IP QE for Display QE for Camera QE for UART QE for Current Consumption QE for Capacitive Touch QE for AFE
RA family lens lens lens lens lens
RE family lens
RX family lens lens lens lens lens lens (Note2) lens
RL78 family lens lens lens lens
RH850 family
RZ family lens lens
Renesas Synergy lens

lens Supported | — Not supported

Notes
  1. For details of Renesas MCUs, refer to the Product Info page for the individual products.
  2. The E2 emulator is under development so that JTAG connection is supported for the current measurement. Use FINE connection for the measurement.
  3. Before using QE for BLE, see the “Solution Toolkit” table on the “Operating Environments for the Latest Versions of Tool Products” page and check that you have selected the type of QE for BLE that is correct for the family of the target MCU and are using a version of the e² studio which supports the given type of QE for BLE.