Nov 8, 2025
About This Video
The Key Setting Tool is a user-friendly utility for securely registering keys based on the SHE standard. It enables easy execution of M1 to M5 calculations, key registration, and verification of registered key information through a simple GUI. Complex processes, such as the Key Derivation Function (KDF), can be performed with a single click. The tool supports key lengths of 128, 192, and 256 bits for added convenience. Note: NDA is required for use.