Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

Updated: Jul.31,2024
Renesas Electronics Corporation

[Product Overview]

This product provides OpenCV Accelerator Support Package for RZ/V2MA.
Please read the Release Note included in this first when you use the package.

[Functions]

  • OpenCV Accelerator Software

[Target Reference Boards]

RZ/V2MA Evaluation Board Kit

[History]

Jul.31,2024:OpenCV Accelerator Support Package V1.40
Jul.31,2023:OpenCV Accelerator Support Package V1.30
Mar.31,2023:OpenCV Accelerator Support Package V1.20
Jan.31,2023: OpenCV Accelerator Support Package V1.10
Sep.29,2022: OpenCV Accelerator Support Package V1.00

[Note]

The following packages is required to use this product.

[Downloads]

Document

Package

[Support Policy]

Renesas provides support for the items below for OpenCV Accelerator Support Package without additional payment.

 FormQ&A and issue analysis*1Maintained by Renesas
Renesas reference boardCustomer board
Customer developed/modified SW-NoNo*2No
Customer added OSS-NoNoNo
Validation target OSS in VLPSource CodeYesNoNo
Renesas developed SWSource CodeYesYesYes
BinaryYesYes*3Yes

*1) Firstly, customers should investigate which part has a problem: Renesas’ deliverables or customer’s developed part.

*2) We provide support for the board-dependent changes such as channel numbers and pin configurations.

*3) We provide Q&A support only for the functions which are defined and described in the user's manual.

Target Devices

Support