Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Overview

Description

Renesas offers a production test and programming unit that enables you to reduce the time to ramp up at a lower cost. The Connectivity Production Line Tool (PLT) is a flexible platform that helps to increase throughput in volume test and programming of units centered around Renesas Connectivity ICs.

The Connectivity PLT is designed to test, calibrate, and perform memory operations for multiple devices under test (DUTs) in parallel. Up to four PLT boards, each with eight test sites, can be daisy-chained to support 32 simultaneous test sites.

Features

  • Up to 32 parallel programming and testing
  • Flexibility in programming OTP/Flash/eFlash
  • Ease of integration: CLI tool included
  • Modular approach: Bluetooth® Low Energy (LE), Wi-Fi, DECT
  • Included tests:
    • Xtal trimming
    • Sensor test
    • GPIO test
    • RSSI test
    • Current measurement
    • Many more
  • Customizable test steps

Target Devices

Downloads

Documentation

Design & Development

Related Boards & Kits

Models

Videos & Training

News & Blog Posts

Support

Support Communities

  1. Production on RA6W1

    Hi Renesas,When I get to the production stage for the RA6W1 will I have to use the Renesas Flash Programmer (Programming GUI) | Renesas ?Can I modify it to support the UART interface for programming?Do you have any adapters for production lines with this tool?Thank you

    Dec 24, 2025
  2. DA14535MOD Codeless without a Dev Kit

    I have previously used the DA14535MOD module with the DA1453x Devkit, running several examples as per your documentation.But now I have to use the DA14535MOD without the Devkit, connected to an RA6M3 microcontroller.  Some questions: I understand that SmartBoot is loaded as a secondary bootloader automatically at power on ...

    Nov 29, 2025
  3. UUID and broadcast name

    ... from keil with the specific UUID and Advertising name ? We have changing this settings from keil project and build the project then flash the board with smartsnipets toolbox with jtag But it takes to much time when you have 5000 boards to give adress and names. Thanks in advance, Marios

    Sep 5, 2018
View All Results from Support Communities (212)