Skip to main content

Renesas Blog

 The IoT Cloud Connection Decision: Wi-Fi or Cellular?

The IoT Cloud Connection Decision: Wi-Fi or Cellular?

With the ubiquity of wireless connectivity options on IoT devices, connection to the cloud has become more flexible than ever. Traditionally, Wi-Fi has been the most popular choice in the IoT world although this has changed in recent years with the huge strides made in cellular networks. However, there is no right answer for which option would be the best or the more efficient between the two.

The type of network connection to use depends on several factors that affect solution development.

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

Power Your Edge AI Application with the Industry’s Most Powerful Arm MCUs

The AIoT has been enabled by higher MCU compute capability and thin neural network models that are more suited for edge and end point devices than traditional CPUs and MPUs.

Renesas Initiatives in Smart Agriculture - Part 1

Renesas Initiatives in Smart Agriculture - Part 1

Introduction to Renesas solutions for smart agriculture

Closing the Performance Gap Between DRAM and AI Processors

Closing the Performance Gap Between DRAM and AI Processors

Blog discussing Renesas’ memory interface solutions

Let's Create a Digital Angle Meter Using a Microcontroller

Let's Create a Digital Angle Meter Using a Microcontroller

We’ll create a digital angle meter using the RL78/G15 Fast Prototyping Board. The data from the gyro sensor will be converted into angles and displayed on the LCD.

Introducing An Easy Tool for Touch Development Even with Partner IDE Platforms

Introducing An Easy Tool for Touch Development Even with Partner IDE Platforms

By using the standalone version of QE for Capacitive Touch, you can develop capacitive touch applications even with IAR's EWRX IDE.

Real-time Vision AI Runs at the Size of a Raspberry Pi! Introducing the RZBoard V2L Single Board Computer

Real-time Vision AI Runs at the Size of a Raspberry Pi! Introducing the RZBoard V2L Single Board Computer

Introducing the RZBoard V2L, a small single-board computer that enables easy Vision-AI trial with the RZ/V2L MPU.

Dynamics of Industrial Field Communication

Dynamics of Industrial Field Communication

Industrial field communication (IFC) facilitates data exchange and real-time decision making during digital transformation in industrial processes, improving efficiency and productivity.

R-Car V3H - Energy Efficient Interior Monitoring Solution (DMS/OMS)

R-Car V3H - Energy Efficient Interior Monitoring Solution (DMS/OMS)

How to implement standalone interior monitoring ranging from a single IR sensor for strictly minimum mandatory features up to multiple sensors with premium features.

RX Family Software – The Past and the Future - #11 Navigating the TCP/IP Implementation Challenges with RX Family

RX Family Software – The Past and the Future - #11 Navigating the TCP/IP Implementation Challenges with RX Family

In this blog, we discuss the approach to implementing network software on MCUs of around 100MHz, specifically those in the RX 32-bit MCU family.