Skip to main content
Renesas Electronics Corporation - June is Pride Month, a month to raise awareness of the rights and the culture of the LGBTQ+ community

Touch System Selection for Cost Reduction and Low-Power Consumption

Image
Masashi Takemura
Masashi Takemura
Sr. Staff Engineer, Product Marketing
Published: September 17, 2025

Making Capacitive Touch Practical with the RA0L1 MCU

Capacitive touch technology is everywhere, from smart locks in office buildings to industrial panels in factories, and microwave ovens to washing machines in homes. As it becomes more common, designers face a familiar set of pressures: deliver a sleek user experience at the lowest possible cost, reduce environmental impact through lower power consumption, and keep designs simple enough to bring products to market quickly.

The RA0L1 MCU was built with these exact challenges in mind. By integrating capacitive touch into a 32-bit, low-end Arm® MCU, it helps product teams streamline their designs, cut costs, and achieve better efficiency without sacrificing performance.

Reducing Cost and Complexity

Traditionally, adding touch required a separate IC plus extra circuitry for features like LED indicators. That meant more components, larger board sizes, and higher BOM costs. The RA0L1 removes this burden by combining capacitive touch and constant-current LED control directly into the MCU, eliminating the need for additional ICs and external resistors. Fewer parts not only lower system costs but also make it easier to shrink product size, a key advantage in space-constrained designs.

Image
RA0L1 BoM Cost Reduction Diagram
Figure 1. RA0L1 BoM Cost Reduction

Optimizing for Low Power

Power consumption is another critical factor, especially in devices that spend long periods waiting in standby mode. The RA0L1's touch engine supports Multiple Electrode Connection and Automatic Judgment, which minimize energy use during idle states while ensuring fast and reliable detection when the user interacts. This balance allows products to stay highly responsive while extending battery life and meeting today's energy efficiency demands.

Image
RA0L1 Capacitive Touch Featured Functions Diagram
Figure 2. RA0L1 Capacitive Touch Featured Functions

Accelerating Development

Integrating new technology often comes with a steep learning curve, but the RA0L1 makes touch implementation straightforward. Renesas provides an evaluation kit with both an RA0L1 CPU board and an application board featuring buttons, wheels, and sliders that mimic real-world use cases. Together with intuitive software tools, this allows engineers to prototype quickly, validate designs, and move confidently into production.

Image
RA0L1 Capacitive Touch Evaluation System Image
Figure 3. RA0L1 Capacitive Touch Evaluation System

Designed for Real-World Needs

By embedding essential functionality into a single device, minimizing power consumption, and offering ready-to-use evaluation resources, the RA0L1 directly addresses the pain points engineers encounter when designing touch-enabled products. From industrial systems to everyday home appliances, it enables smarter, smaller, and more efficient designs—helping manufacturers meet cost targets and environmental goals without compromising user experience.

Learn more about how the RA0L1 can simplify your next design: renesas.com/ra0l1.