Skip to main content
Renesas Electronics Corporation

Overview

Description

The debugging MCU board is a board to enable the in-circuit connection of an emulator with the user's system and allows you to use more enhanced debugging functions. The applicable debugging functions vary depending on the MCU type.

Target Devices

Additional Details

Lineup

E2 Emulator

E1 Emulator

E20 Emulator

E10A-USB Emulator

Information on the discontinuation of E1 emulator production and on its successor products

We have already discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.

>> Tool News: [Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

Support

Support Communities

  1. how to buy or free use cs++

    Dear friend I using multi compiler to output elf/hex file. Question: Can i use CS++ load thes elf/hex to board debugging ?MCU:U2A16/RH850/516 pin --------------- regards

    Nov 1, 2024
  2. E2 lite , RL78/G10: R5F10Y16, 10 PIN MCU target board, Debugging

    Hi  can i able to program my RL78/G10 MCU Target board : R5F10Y16-TB directly from E2 Lite emulator using CS+ IDE ? Also, can i able to debug it ?  Actually currently i am not able to do so. Kindly advise.   Regards Harsh Sharma

    Feb 19, 2018
  3. RA2L1 stuck in a reset loop

    Hello, I have a custom board with RA2L1 MCU and debugging it through EK-RA2L1 onboard j-link (via SWD). It was working fine but something happened, I prob. flashed the wrong binary and I can't communicate with the MCU anymore. Seems to me that it's stuck in ...

    Aug 18, 2022
View All Results from Support Communities (725)

Knowledge Base

  1. How to debug the pin functions whose user port is multiplexed with the microcontroller pins used for communication with the on-chip debugging emulator

    ... there is a debugging MCU board for the microcontroller in use, using that debugging MCU board enables debugging of all microcontroller pin functions. (Though a debugging MCU board is also provided for the RH850 family, pin restrictions could not be worked around in the debugging MCU board for the RH850 ...

    Apr 26, 2017
  2. How to debug a program using a pin for the on chip emulator as a user pin?

    Renesas has prepared debugging MCU boards for low pin count package products. Using such a board, a pin assigned to the on-chip emulator signal can also be used as a user pin. In addition, when debugging using a FINE connection, all ports other than the port to which the ...

    Jan 23, 2014
  3. E10A and E10A-USB emulator compatible with SH7147 and SH7142

    The E10A-USB emulator unit cannot be used as is because SH7147 and SH7142 MCUs do not embed debugging functions. However, the SH7417 Debug MCU Board (sold separately) can be used with the E10A-USB emulator to enable debugging. For more information, click here.

    Sep 27, 2017
View All Results from Knowledge Base (14)
Support Communities

Support Communities

Get quick technical support online from Renesas Engineering Community technical staff.
Browse Articles

Knowledge Base

Browse our knowledge base for helpful articles, FAQs, and other useful resources.
Submit a Ticket

Submit a Ticket

Need to ask a technical question or share confidential information?