TOKYO, Japan October 7, 2015 — Renesas Electronics, a premier provider of advanced semiconductor solutions, today announced the availability of the RZ/G microprocessor (MPU) Series, which enables rapid development of high-performance Linux and Android applications. Designed for industrial, home appliances, and office equipment employing a human machine interface (HMI), the RZ/G Series extends the capabilities of the successful RZ/A Series MPUs—which supports 2D graphics at up to WXGA resolution—to deliver high-end performance in applications such as image processing, video sensing, and 3-D graphics and multimedia at up to 1080p resolution.
Key features of the new RZ/G Series:
(1) High performance for enhanced UI expressiveness and video sensing
The new RZ/G Series of MPUs utilizes Renesas' proprietary Full HD video codec (processing up to 1080@60) in addition to the PowerVR™ SGX540 (RZ/G1E) or PowerVR™ SGX544MP2 (RZ/G1M) 3-D graphics core from Imagination Technologies Limited. These intellectual property (IP) blocks make it possible to develop highly effective user interfaces (UI) on products ranging from hand-held medical devices to digital signage by incorporate elements such as simple still images, 3-D graphics, plus video content. This functionality improves UI expressiveness and adds value to new products.
The RZ/G Series is comprised of two product versions: the RZ/G1E with dual ARM® Cortex®-A7 CPU cores operating at up to 1.0 gigahertz (GHz) and the RZ/G1M with dual Cortex-A15 CPU cores operating at up to 1.5 GHz. This range of high-end options lets customers tune their designs for either power or performance. Each RZ/G device includes an 800 megahertz (MHz) DDR3 external memory interface, which provides ample performance margin for applications including image processing of multiple video streams for monitoring systems and video sensing such as face recognition. High-speed interfaces including USB 3.0, PCI-Express, and serial ATA are integrated on-chip, allowing easy expansion of functionality without the need for external components. Functional IP modules and memory map are common over the entire RZ/G Series lineup, so the same drivers and software can be shared among different products in the series, thereby enhancing design scalability.
(2) Hierarchy of support and services provided in collaboration with partners
The RZ/G Series is backed by an ecosystem of Renesas partners that provides system integration services, graphical user interface (GUI) frameworks, middleware, OS support, board design, as well as sales of evaluation and mass-production boards. These products and services help limit the increasing workload and cost associated with hardware and software development of complex, high-end systems. Buoyed by partners like Cogent Embedded, Timesys, Adeneo Embedded, and others - all leaders in embedded open source development with expertise spanning Linux and Android system integration, middleware, and graphical user interface (GUI) support - customers will be able to confidently tackle their next embedded projects and remove 40 percent from their typical development cycle.
RZ/G Series MPUs support Linux 3.10 LTSI, which will let customers develop secure and flexible systems within a proven, industry-standard development flow. Android KitKat support will be available later in 2015, and Linux kernel 4.1 will also be supported. The two available starter kits for the RZ/G1E and RZ/G1M devices will simplify the prototyping process. Each starter kit offers an abundance of connectivity options plus board support package and documentation. With the new high-end RZ/G Series of MPUs, Renesas simplifies complex display and control devices with a world-class integrated software and hardware platform. Board support packages and development kit documentation will be available from www.elinux.org and the RZ/G GitHub site by the end of October 2015.
Availability
Samples of the RZ/G Series of MPUs are available now. Mass production of the RZ/G Series of MPUs is scheduled to begin in July 2016 and is expected to reach a volume of 100,000 units per month in July 2017. (Availability is subject to change without notice.)
Please refer to the separate sheet (PDF: 112 KB) for the main specifications of the RZ/G1E and RZ/G1M MPUs.
For more product information, please visit: https://www.renesas.com/en/products/microcontrollers-microprocessors/rz.html
About Renesas Electronics Corporation
Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.
(Remarks) ARM and Cortex are registered trademarks of ARM Limited (or its subsidiaries) in the EU and in other countries. PowerVR™ is a registered trademark of Imagination technologies Limited (or its subsidiaries) in the EU and in other countries. All registered trademarks or trademarks are the property of their respective owners.
The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.