Grape Systems Inc.
Categories: Communication, Cloud Connection
The ThreadX-µITRON Wrapper allows porting of µITRON-based applications to the ThreadX® RTOS for the Synergy Platform.
It enables ThreadX to be used as a µITRON 4.0 compliant RTOS. It calls ThreadX APIs and allows applications to reuse µITRON assets with Synergy MCUs and make direct ThreadX service calls.
ThreadX-µITRON Wrapper is ideal for applications such as kiosk machines, fire alarm panels, point-of-sale (POS) systems, printers, medical equipment, and various consumer electronics.