Skip to main content
Renesas Electronics Corporation

Intersil's Highly Efficient Buck Controller Supports New Levels of Flexibility for High Current Designs

55V ISL78268 Buck Controller Provides Very High Step-Down Efficiency for Industrial and Automotive Applications

August 4, 2014
 

MILPITAS, Calif., Aug. 4, 2014 (GLOBE NEWSWIRE) -- Intersil Corporation (Nasdaq:ISIL), a leading provider of innovative power management and precision analog solutions today announced the ISL78268 55V synchronous buck controller with 3A integrated high side and low side drivers. The most versatile high voltage buck solution available, the ISL78268 buck controller provides very high step-down efficiency for a wide variety of load currents from under 5 to over 25A, enabling it to support virtually every 12, 24, or 48 volt high current buck requirement for automotive and industrial applications.

A photo accompanying this release is available at http://www.globenewswire.com/newsroom/prs/?pkgid=26851.

 

For heavy load applications, designers often have to balance power conversion efficiency against size and noise constraints. This requires making trade-offs among component selection, switching frequency, and output ripple and often requires the power stage to be tailored to the load in question. The ISL78268 buck solution was designed specifically to be flexible so that it can be used regardless of the optimization balance.

 

The ISL78268 buck controller enables easy conversion from high primary rails (typically 12, 24 or 48V) to lower secondary rails (typically 3.3, 5.0 or 12V). It fully integrates both a peak current mode synchronous PWM controller and a dedicated constant current control loop as well as high-side and low-side FET drivers that have adaptive dead time control. The ISL78268 device's tolerance of 55V inputs makes it ideal for automotive applications, including support for the 12V clamped load-dump specifications and new 48V power system being adopted by European OEMs. The integrated 3A driver allows the ISL78268 buck controller to sharply switch small power FETs or parallel combinations of large FETs while minimizing dead time to reduce switching losses, improve efficiency and reduce excess heat dissipation. This allows a single buck controller to be used across a wide variety of load requirements, simplifying design and reducing time-to-market.

 

"The ISL78268 was designed to enable power conversion with very high efficiency and improved performance over traditional solutions," said Philip Chesley, vice president of Intersil's Precision Products. "The unique combination of features provides customers with a very versatile solution that can be used and re-used across their high voltage designs."

 

  • Supports 5-25A loads and can be used in a two-phase, current sharing configuration to support loads up to 50A
  • 55V input tolerance (60V abs max)
  • Integrated 3A FET drivers and PWM controller for cycle-by-cycle peak current limiting
  • Provides average current limiting to extend battery life in battery charging applications and avoid inductor current runaway in supercap charging applications
  • Adaptive dead-time control to prevent overlap current and minimize body diode conduction losses with varying sized power FETs
  • Selectable diode emulation and burst mode for light loads
  • Adjustable switching frequency from 50kHz to 1.1MHz
  • Low shutdown current of 3uA
  • AEC-Q100 qualified

 

The ISL78268 is available now. Pricing for the ISL78268 buck controller starts at $2.45 USD in 1k quantities. The ISL78268 is offered in a 24 lead 4x4mm QFN package. The ISL78268 is supported by the ISL78268EVAL1Z, evaluation kit available for $83.33 USD each.

 

For more information on the ISL78268 buck controllers, please visit: ISL78268.

 

Intersil and the Intersil logo are trademarks or registered trademarks of Intersil Corporation. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.