Platform

※ The document for RZ/G2 is under preparation. For inquiries, please contact Renesas Electronics sales office or Contact US.

Title Overview
RZ/G2 Group Linux BSP Porting Guide This guide explains how to port a RZ/G2 Linux BSP to a custom board based with a RZ/G2 group device.

Hardware Manuals

Title Overview
RZ/G2H Overview This is a overview of the hardware specification of the RZ/G2H processor.
※ User's Manual is under preparation. For details, please contact Renesas Electronics sales office or Contact US.
RZ/G2M Overview This is a overview of the hardware specification of the RZ/G2M processor.
※ User's Manual is under preparation. For details, please contact Renesas Electronics sales office or Contact US.
RZ/G2N Overview This is a overview of the hardware specification of the RZ/G2N processor.
※ User's Manual is under preparation. For details, please contact Renesas Electronics sales office or Contact US.
RZ/G2E Overview This is a overview of the hardware specification of the RZ/G2E processor.
※ User's Manual is under preparation. For details, please contact Renesas Electronics sales office or Contact US.
RZ/G Series User's Manual & Technical Update This is the user’s manual for the RZ/G-PF series of processors that are compatible with the RZ/G Linux Platform.
The product line includes the RZ/G1H-PF, RZ/G1M-PF, RZ/G1N-PF, RZ/G1E-PF, and RZ/G1C-PF.
Technical update can also be obtained together, so please read it in conjunction there.
RZ/G1H-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1H-PF processor that support the RZ/G Linux Platform.
Technical update can also be obtained together, so please read it in conjunction there.
RZ/G1M-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1M-PF processor that support the RZ/G Linux Platform.
Technical update can also be obtained together, so please read it in conjunction there.
RZ/G1N-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1N-PF processor that support the RZ/G Linux Platform.
Technical update can also be obtained together, so please read it in conjunction there.
RZ/G1E-PF User's Manual & Technical Update These are the hardware specifications for the specific parts of the RZ/G1E-PF processor that support the RZ/G Linux Platform.
Technical update can also be obtained together, so please read it in conjunction there.
RZ/G1C-PF User's Manual & Technical Update There are the hardware specifications for the specific parts of the RZ/G1C-PF processor that support the RZ/G Linux Platform.
Technical update can also be obtained together, so please read it in conjunction there.

Verified Linux packages

Title Overview
RZ/G2 Yocto recipe Start-Up Guide This manual explains how to build the Linux kernel for the RZ/G2 by using Yocto build system.
RZ/G2 Group BSP Manual Set This is the set of user manuals that cover the driver module functions and interface specifications for controlling the hardware mounted on RZ/G2 products.
RZ/G Verified Linux Package Start-Up Guide Whole steps to use RZ/G Verified Linux Package on the reference board are described.
RZ/G1 Yocto recipe Start-Up Guide This manual explains how to build the Linux kernel for the RZ/G1 by using Yocto build system.
RZ/G1 Group BSP Manual Set This is the set of user manuals that cover the driver module functions and interface specifications for controlling the hardware mounted on RZ/G1 products.

Application Notes/Other

Title Overview
RZ/G2 Group Application Note This application note introduces example applications that run on the RZ/G2 products.
RZ/G1 Group Application Note This application note introduces example applications that run on the RZ/G1 products.
RZ/G Qt User Guide About the open source version of Qt which is included in Verified Linux Package are described.
RZ/G Linux Platform Customization Guide How to change the items that are often customized with the RZ/G validated Linux package is described.
RZ/G Linux Platform Developer's Guide Development know-hows on RZ/G Verified Linux Package are described.