Overview

Description

Clarinox Technologies Pty Ltd.

Categories: Wireless

Uses the ClarinoxBlue Bluetooth® protocol stack and the Joeyduino™ Shield wireless module to enable pairing and bidirectional data transfer between the Synergy S7 MCU-based Kit and nearby BLE devices.

The application can be run in either BLE central mode to scan and connect with other BLE peripherals, or in BLE peripheral mode to advertise to nearby BLE central devices. A smartphone running a BLE central app, such as the nRF Connect app for Android or LightBlue for iOS, can connect to the Synergy Kit for bidirectional data transfer.

The ClarinoxBlue stack includes a built-in protocol analyzer for simplified debugging that allows custom application commands to be sent using the DLL-based plug-in interface. It offers threading, memory usage and memory leak analysis, and an API for messaging between processors.

Release Information

Copyright Disclaimer

Copyright 2017 Clarinox Technologies Pty Ltd. All Rights Reserved.

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

Synergy Download

Clarinox BLE Central and Peripheral

1.0.0

Current Public Release

Release Date:2017-06-23

MCUs Supported: S7G2

MD5: 5a0d34d4f862f385663a842d7b010e3b

What's New?

N/A

Installation Instructions

This application has the following hardware requirements:

  • Renesas Synergy SK-S7G2 kit
  • Clarinox Joeyduino Shield Wireless module
  • Smart Phone or mobile device

Installation instructions are included in the application project guide.