The Importance of Reference Documentation for Consumers and Engineers
In this blog, we examine the differences in documentation needs between consumer products and engineering products.
In this blog, we examine the differences in documentation needs between consumer products and engineering products.
Softwareにより車の価値を定義するSoftware defined vehicleにおいては新しいアプリケーション をさまざまな車種へ搭載する事が求められます。このため、デバイスを意識することなくアプリケーションを開発することができるソリューションの開発に取り組んでいます。
大規模化・複雑化するE/Eアーキテクチャの早期に開発に向けて、実機無しでデバイス間通信を伴うソフトウェア開発を可能とする、「マルチデバイス用協調シミュレーション環境」を提案します。
高精度ΔΣADC内蔵MCU RX23E-Aがセンサ機器の共通化に貢献した実例を二回に分けてご紹介します。初回の今回は、同一製品間での共通化にスポットを当てます。
このブログでは、ルネサスが自動車業界の進化をどのように捉え、事業戦略を描くか、ご紹介します。
How we can use the Data Operating Circuit and the Data Transfer Controller to create complete, autonomous subsystems that can make simple decisions based on measured data without CPU intervention.
Multiplexed Register Clock Driver (MRCD) and Multiplexed Data Buffer (MDB) components allow DDR5 memory modules to deliver significantly higher bandwidth for memory sub-systems in next-generation servers.
Renesas offers a solution that adapts well in remote locations where there is no Wi-Fi or Bluetooth LE access, only a cellular radio using CAT-M1; the inclusion of solar energy harvesting into the design allows for long-term battery life.
最新マイコンRX140が搭載するCTSU2SLの新機能を活用した自己容量耐水ソリューションにより、基板サイズの制約がある水回り用途でも静電容量式タッチキーを実現できます。