メインコンテンツに移動
ルネサス エレクトロニクス株式会社 (Renesas Electronics Corporation)

ブログ

Power Up Your SPI Transfers

Power Up Your SPI Transfers

This blog looks at how we can automate a series of SPI transfers using the command sequencer implemented on many RA 32-bit MCU devices.

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution? Blog

Looking for a Reliable, Ready-to-Use Gigabit Industrial Ethernet Solution?

Gigabit speed and its associated frequencies require sophisticated schematics and PCB design. Renesas’ Gigabit Industrial Ethernet SoM solution contains all of the needed mission-critical components.

Reducing Noise Issues in Microcontroller Systems Blog

Reducing Noise Issues in Microcontroller Systems - Part 4

In this blog, we look at some of the features implemented on RA microcontrollers that can help create reliable applications in the face of noise.

RH4Z2501: The New Robust IO-Link Compliant Transceiver

RH4Z2501: The New Robust IO-Link Compliant Transceiver

The IO-Link protocol (IEC 61131-9) is getting a lot of traction within the factory and process automation sector.

Renesas AI Panel Recap: Semiconductor Industry Is Pulling AI Across a Diversity of End Uses and Applications

半導体産業が多様な用途と応用でAIをリードする

半導体を活用してAIが普及していく期待と、半導体業界の中で設計やテストにAIが活用されている現状と展望を、キーマンらがパネルディスカッションした内容を紹介します。

 Accelerate Your Automotive Innovations with the R-Car S4 SoC Low Cost Evaluation Board Starter Kit Blog

Accelerate Your Automotive Innovations with the R-Car S4 SoC Low-Cost Evaluation Board Starter Kit

As the automotive industry is challenged to introduce software-defined vehicles (SDVs), it is crucial to have a low-cost and easy-to-use development environment for rapid software development.

Introducing the Handbook that Provides a Comprehensive Overview of RX140!

RX140のすべてが一目で分かるハンドブックのご紹介!

本ハンドブックでは、製品開発時に必要な資料やツール等を開発フェーズごとに纏めて一覧にしています。ユーザーは豊富なコンテンツの中から最適な情報をすぐに把握できます。

Giving Customers the Options to Make or Buy SoM and/or SBC to Accelerate Design Cycle

SOM/SBCの製造または購入という選択肢が、顧客の設計サイクルを加速させます

システムオンモジュール(SOM)やシングルボードコンピュータ(SBC)を使用する主な利点は、必要な知識やリソースを分割できることです。開発サイクルの加速に役立つ、すぐに使えるSOMとSBCの利点を詳しく掘り下げてみていきます。 

Ethernet Evolution for Industrial Applications

産業用アプリケーションにおけるイーサネットの進化

産業用イーサネットは、インダストリー4.0の決定論とリアルタイム制御を可能にするさまざまなネットワーキング・プロトコルをサポートし、重要な役割を果たしています。

Why Use a Power MUX Load Switch for Seamless Switchover Between Power Rails blog

Why Use a Power MUX Load Switch for Seamless Switchover Between Power Rails

With the ever-increasing power requirements of electronic devices, efficient power management has become a necessity. Power MUX load switches are one of the innovative solutions that aid effective power management.