Skip to main content

Renesas Blog

Evolution of sensing equipment and force sensor measurement using RX23E-A

Evolution of Sensing Equipment and Force Sensor Measurement Using RX23E-A

A force sensor can be mounted to the tip of a robotic arm to measure load and torque. This blog introduces the Application Note on force sensing measurement using the RX23E-A 32-bit MCU.

Changes in Automotive E/E Architecture and Semiconductor Initiatives in the CASE+E Era

Japan IT Week特別講演「CASE+E時代における車載E/Eアーキテクチャの変化と半導体への取組み」

CASE+Eのこれからの自動車業界において半導体

に求められる価値提供、及び当社のアプローチをご紹介します。

Selecting the Best Device for Converter Clocking Applications

This blog helps customers find the right devices to use when they are looking for a high-performance clock to drive their data converters.

SparkFun’s new Qwiic Wi-Fi Shield uses Renesas’ DA16200 Module

SparkFun's New Qwiic Wi-Fi Shield Uses Renesas’ DA16200 Module

The Qwicc Wi-Fi Shield based on Renesas’ Wi-Fi DA16200 module, is an Arduino Uno R3 form factor shield that enables rapid development of ultra-low power Wi-Fi IoT applications.

Renesas’ DA16200 wins China IoT Innovation Award 2020

Renesas' DA16200 Wins China IoT Innovation Award 2020

Renesas' DA16200 Wi-Fi System-on-Chip (SoC) and modules have won the Communication Technology category at Elecfans' annual China IoT Innovation Awards.

Provisioning App Blog image

Renesas Wi-Fi Provisioning App is Available Now on Google and Apple Stores

Renesas’ Wi-Fi Provisioning App, a mobile application that works with development kits supported by the DA16200 and DA16600 Wi-Fi SoCs, is now available for use on Google Play and Apple Stores.

FreeRTOS Support for Its Ultra-low Power DA16200 SoC Blog Image

Renesas Introduces FreeRTOS Support for Its Ultra-low Power DA16200 SoC

Renesas offers FreeRTOS support for the DA16200, a real-time operating system for MCUs that helps to program, use, secure, connect, and manage small, low-power edge devices without extra effort.

Multi-Cell USB-PD + QC2 & QC3 Power Bank Blog

Multi-Cell USB-PD and PPS Power Bank with Qualcomm Quick Charge and OS Independent Monitoring

/node/1601921This is a detailed description of a solution for a multi-cell USB Power Delivery (USB-PD) enabled power bank using a 2S to 4S battery stack that supports USB-PD 3.0, PPS and Qualcomm Quick Charge.

Develop Faster Using Example Projects for RA MCU Innovation Kits for IoT

Develop Faster Using Example Projects for RA MCU Innovation Kits for IoT

Users of RA MCU innovation kits for IoT can utilize 600+ example projects as building blocks to create feature-rich IoT and embedded proof-of-concepts quickly and easily.

Quickly Programming RA MCU Innovation Kits for IoT

Quickly Programming RA MCU Innovation Kits for IoT

This blog provides useful information on programming a pre-built hex file onto an RA kit using Renesas Flash Programmer and Segger® J-Flash Lite without having to build the source code or use an IDE.