Flexible Interface of the ZSSC3241 Enables Bridge as Temperature Sensor
The advanced features of the ZSSC3241 SSC enable using the bridge sensor as a thermometer for temperature compensation.
The advanced features of the ZSSC3241 SSC enable using the bridge sensor as a thermometer for temperature compensation.
If you want to use RA2 microcontrollers but don't know where to start, we have good news for you. If you follow this blog, you will be able to set up the RA2 microcontroller development environment and even operate the HS3001 temperature sensor.
Industrial networking for IoT devices is quite diverse. Renesas offers comprehensive solutions for high-performance MCUs, A&P portfolios, SW platforms, and tools to drive industry 4.0.
Power modules have been a great option for engineers for many years and through technological advances, suppliers are increasing their benefits in terms of size, ease-of-use and flexibility.
Our solution utilizes the advanced security feature of RX, the Trusted Secure IP, to establish the Root of Trust, which is crucial for ensuring the security of IoT devices.
The importance of quality and reliability in the context of embedded designs cannot be overstated. Read an overview highlighting the decades of Renesas commitment to building quality into our MCU design from concept through production.
Developers of wireless IoT device networks and smart meters can overcome their challenges with this wide-area, high-speed wireless communication Wi-SUN FAN 1.1 solution embedding Sub-GHz wireless communication.
This blog introduces the features and benefits of RX66T-Based Whole Speed Range Position Sensorless FOC.
Read about the latest addition of BGA package options to the RA4M3/RA6M4/RA6M5 group of MCUs and how these smaller packages are enabling new use cases.
The RAA211x family of scalable integrated FETs (up to 5A) & high voltage (up to 75V) peak-current mode switching regulators provides easy-to-use multipurpose solutions to meet your power requirements.