メインコンテンツに移動

ブログ

Things to Consider When Developing an ASIC Blog

Things to Consider When Developing an ASIC

Due to the non-homogenous nature of IIoT requirements, one size does not fit all in the IIoT. ASICs offer many advantages to a customer and working with the correct supplier is key to achieving these benefits.

Simplifying Smart Home with an Ultra-Low Power Wi-Fi Platform Blog

Simplifying Smart Home with an Ultra-Low Power Wi-Fi Platform

Low power Wi-Fi technology will make the smart home network a lot simpler by eliminating the need for an expensive hub and solving the issue of protocol fragmentation.

Condition Monitoring ASICs Extend Systems’ Lifetime Blog

Condition Monitoring ASICs Extend Systems’ Lifetime

With an ASIC solution, all the condition monitoring circuitry can be placed on the same chip with all the required electronics for the core function of the product.

Successful Debugging Requires Bridging the Hardware-Software Gap Blog

Successful Debugging Requires Bridging the Hardware-Software Gap

Debugging is an important part of embedded design; one that requires bridging the hardware/software gap.

Ubiquitous Broadband Communications Blog

Ubiquitous Broadband Communications

Renesas is making this IP accessible to manufacturers looking to develop a custom IC. This will enable wireless broadband access to flourish and bring the internet to every part of the global population.

RX - The Road Ahead!

RXのこれから

10年以上前、誰もがArmコアのライセンスを持っていた当時、私たちは反対を受けつつも覚悟を決めルネサスRX (Xtreme) マイクロコントローラの開発に挑戦しました。そのRXも昨年10周年を迎え、喜ばしい事に累計出荷台数10憶台到達という非常に重要なマイルストーンを達成することができました。

The Art of Networking (Series 7): TSN in a Virtualized Environment

The Art of Networking (Series 7): TSN in a Virtualized Environment

Here, we show solutions for Precision Time Protocol (PTP) time distribution to virtualized OS with the help of hardware-assisted virtualization (Renesas R-Switch2) to solve challenges quickly.

Blog image ADAS/AD

E/Eアーキテクチャ向けSW Platform と開発環境シリーズ(10);ADAS/AD 画像認識ソフトウェア開発 (ソフトウェアにより自動運転社会の実現に貢献)

高度な自動運転社会の実現に向けて、画像認識ソフトウェアの開発、機能安全に対応した自動運転プラットフォームの提供に取り組んでいます。

E/Eアーキテクチャ向けSW Platform と開発環境シリーズ(11);インフラストラクチャ (E/Eアーキテクチャ向けソリューション提案により、新たなモビリティ社会を実現)

私たちインフラストラクチャーチームは、開発者が必要とする開発環境、CI/CD (継続的インテグレーション・継続的デリバリー)やツールの提供だけでなく、顧客・マーケティング部門・品質保証/品質管理部門と一体となって効率的なソフト開発のバリューチェーンを実現するインフラ開発を行っています。

Blog image RADAR solutions for automotive

E/Eアーキテクチャ向けSW Platform と開発環境シリーズ(9);RADARソリューション開発

運転支援や自動運転分野において、車両周辺の認識センサー技術が非常に重要となってきます。今回、認識センサを代表するRADARについての取り組みを紹介します。